Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: ADI’s Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Other Products (EN)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other Products (EN)
Other Products (EN)
Documents Turning the potentiometers on the EV board does not change the input to the MAX1464. What is the problem?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD10200: FAQ
  • +AD8436: FAQ
  • 3B01: the connection between the 26-pin and 16 channel.
  • 442 - I cannot find the datasheet for the 442 (old OPAMP Module)
  • 751: old datasheet
  • Ac coupling Vs Dc coupling
  • AC1307E Power Supply input range
  • AD-MSDPD-EVB: Eval Board Datasheet
  • ADATE304 Force Voltage
  • ADATE318: What supply voltage do I use for VDD_THERM?
  • ADMP401 startup
  • ADMP441 output format
  • +ADN2531: Can output be configured as current source?
  • ADN2685: could you send the final datasheet?
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • ADN2817 error correction
  • ADN2820: Optical fiber communication
  • +ADN2830: FAQ
  • +ADN2871: Differential drive circuit for driving a VCSEL Laser diode.
  • +ADN2872: Is it possible to use 2 laser drivers in parallel to have the modulation current of 130 mA?   
  • ADN2873: Minimum differential signal between the DATAP and DATAN
  • ADN2880: MAX leakage current specification of ADN2880 input
  • +ADN2882 Evaluation Board
  • +ADN4600: FAQ
  • +ADN469xE: FAQ
  • +ADN8831: FAQ
  • ADN8834: Evaluation board difference
  • AN-695 Q&A
  • Aqueous washing of ADI parts?
  • Baking BGA in Tray or trays
  • Baking of parts in a Reel
  • Can ADN4604 do single ended 75Ohm input and output?
  • Can I connect one input to multiple outputs?
  • datasheet 2B35
  • Digital programmable power with 1.8V logic to Vout = 5V
  • Does changing the crosspoint connectivity affect the state of previously configured connections?
  • doubling ADN8810 Iout configuration query (SR#: 1202803)
  • EVAL-AD8436 evaluation board operation with single supply
  • Failure probability for AD8468
  • How can I order Linear Circuit Design Handbook?
  • Maximum Recommended PMU Load Capacitance
  • MTBF-reliability data
  • Package general: What is the pin pitch of LFCSP package?
  • Package: 10 ld Ceramic Flat Package footprints
  • paste mask recommendation
  • PFC controller + LED driver in one package
  • Replacement for PMI119-883
  • RoHS compliant status E
  • RTI-850 RTI products
  • Shelf life for Analog parts
  • Shelf life of drypack used to ship Moisture/Reflow Sensitive Surface Mount Devices
  • The unit of MTTF data on ADI web site
  • transistor counts for a processor to calculate the MTBF
  • unused inputs or outputs?
  • What data rates or range of data rates are supported?
  • What data rates protocols are supported?
  • Where can I find e-book versions on your seminar books to download?
  • which register we can read to know the status of HD
  • Why the Analog Input Current from ?10mA to 10 mA was limited.
  • +#N/A: FAQ
  • +--: FAQ
  • +1-WIRE + I2C MULTI-DEVICE PROGRAMMER: FAQ
  • +125932-HMC675LP3E: FAQ
  • 1s74: FAQ
  • +310: FAQ
  • +73M1X22: FAQ
  • +73S8010C-ILR/F: FAQ
  • +78P2351-IGT: FAQ
  • +78Q2123/F: FAQ
  • +78Q8392LA03-CHR/F: FAQ
  • +940: FAQ
  • +AD-CELLPACKBM-SL: FAQ
  • +AD-GMSL522-SL: FAQ
  • AD1835: FAQ
  • +AD1835A: FAQ
  • AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1862: FAQ
  • +AD1881A: FAQ
  • +AD1937: FAQ
  • +AD1938: FAQ
  • +AD1939: FAQ
  • +AD1970: FAQ
  • AD1981: FAQ
  • +AD1981B: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +AD22151: FAQ
  • +AD22282-A-R2: FAQ
  • +AD22290: FAQ
  • +AD506: FAQ
  • +AD53500: FAQ
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD598JRZ: FAQ
  • +AD630: FAQ
  • +AD644: FAQ
  • +AD6635: FAQ
  • +AD671: FAQ
  • +AD7124: FAQ
  • +AD7280: FAQ
  • +AD73311: FAQ
  • +AD73311L: FAQ
  • AD73322: FAQ
  • +AD73322L: FAQ
  • +AD74111: FAQ
  • +AD7503: FAQ
  • +AD7546: FAQ
  • +AD7725: FAQ
  • +AD7756: FAQ
  • +AD8036: FAQ
  • +AD8041: FAQ
  • +AD8042: FAQ
  • +AD8045: FAQ
  • +AD8051: FAQ
  • +AD8074: FAQ
  • +AD8075: FAQ
  • +AD811: FAQ
  • +AD8128: FAQ
  • +AD8129: FAQ
  • +AD8130: FAQ
  • +AD8134: FAQ
  • +AD8145: FAQ
  • +AD8321: FAQ
  • +AD8328: FAQ
  • +AD8380: FAQ
  • +AD8381: FAQ
  • +AD8460: FAQ
  • +AD846: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9631: FAQ
  • +AD9776: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9882: FAQ
  • +AD9910: FAQ
  • +AD9911: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +ADA4302-4: FAQ
  • +ADA4355: FAQ
  • +ADA4411: FAQ
  • +ADA4853-2: FAQ
  • +ADAU1381: FAQ
  • +ADAU1461: FAQ
  • +ADAU1701: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADCMP580BCPZ-RL7: FAQ
  • +ADE5569: FAQ
  • +ADE7752: FAQ
  • +ADE7753: FAQ
  • +ADE7754: FAQ
  • +ADE7756: FAQ
  • +ADE7757: FAQ
  • +ADE7758: FAQ
  • +ADE7761: FAQ
  • +ADE7763: FAQ
  • +ADE7816: FAQ
  • +ADE7854: FAQ
  • +ADE7858: FAQ
  • +ADE7868: FAQ
  • +ADE7878: FAQ
  • +ADE7880: FAQ
  • +ADE7953: FAQ
  • +ADE7978: FAQ
  • +ADE9078: FAQ
  • +ADE9113: FAQ
  • +ADE9430: FAQ
  • +ADF4360: FAQ
  • +ADF5584: FAQ
  • +ADF7001: FAQ
  • +ADF7012: FAQ
  • +ADF7020: FAQ
  • +ADF7021-N: FAQ
  • +ADF7021-V: FAQ
  • +ADF7023: FAQ
  • +ADF7242: FAQ
  • +ADF7902: FAQ
  • +ADG201: FAQ
  • ADG324x Level Translation: high to low
  • +ADG623: FAQ
  • +ADIN6310: FAQ
  • +ADIS16204: FAQ
  • +ADIS16300: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16480: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADISIMPLL: FAQ
  • +ADISUSB: FAQ
  • +ADL5317: FAQ
  • +ADM1030: FAQ
  • +ADM1031: FAQ
  • +ADM1060: FAQ
  • +ADM1062: FAQ
  • +ADM1064: FAQ
  • +ADM1066: FAQ
  • +ADM1068: FAQ
  • +ADM1069: FAQ
  • +ADM1166: FAQ
  • +ADM1171: FAQ
  • +ADM1175: FAQ
  • +ADM1186: FAQ
  • +ADM3307: FAQ
  • +ADM869L: FAQ
  • +ADMC300: FAQ
  • +ADMTV315: FAQ
  • +ADMV4420: FAQ
  • +ADN2892: FAQ
  • +ADP1047: FAQ
  • +ADP1048: FAQ
  • +ADP195: FAQ
  • +ADP198: FAQ
  • +ADP3040: FAQ
  • +ADP3302: FAQ
  • +ADP3623: FAQ
  • +ADP3624: FAQ
  • +ADP5046: FAQ
  • +ADPA1112: FAQ
  • +ADPA9007: FAQ
  • +ADR125: FAQ
  • +ADRF5162: FAQ
  • +ADRF5700: FAQ
  • +ADRF6515: FAQ
  • +ADRV9002: FAQ
  • +ADRV9003: FAQ
  • +ADRV9026: FAQ
  • +ADRV9361-Z7035: FAQ
  • +ADRV9361: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21365: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +ADSP-BF533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF701: FAQ
  • +ADSP-CM408F: FAQ
  • +ADSP-TS001: FAQ
  • +ADT70: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +ADUC7020: FAQ
  • +ADUC7021: FAQ
  • +ADUC7023: FAQ
  • +ADUC7024: FAQ
  • +ADUC7026: FAQ
  • +ADUC7033: FAQ
  • +ADUC7060: FAQ
  • +ADUC7061: FAQ
  • +ADUC7120: FAQ
  • +ADUC7122: FAQ
  • +ADUC7126: FAQ
  • +ADUC7128: FAQ
  • +ADUC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADUC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADUC836: FAQ
  • +ADUC841: FAQ
  • +ADUC842: FAQ
  • +ADUC843: FAQ
  • +ADUC845: FAQ
  • +ADUC847: FAQ
  • +ADUC848: FAQ
  • +ADUCM360: FAQ
  • +ADUCM361: FAQ
  • +ADUCM362: FAQ
  • +ADUCM4050: FAQ
  • +ADUCM410: FAQ
  • +ADUCRF101: FAQ
  • +ADV7202: FAQ
  • +ADXL358: FAQ
  • +ADXL365: FAQ
  • +CABLE-PH04: FAQ
  • +CN0196: FAQ
  • +CN0287: FAQ
  • +CN0303: FAQ
  • +DC1075B-B: FAQ
  • +DC1854A: FAQ
  • +DC2039A: FAQ
  • +DC2046A-B: FAQ
  • +DC2393A: FAQ
  • +DC2465A: FAQ
  • +DC2617A: FAQ
  • +DC9000A: FAQ
  • +DC9018A-C: FAQ
  • +DC9021B: FAQ
  • +DC9022B: FAQ
  • +DS1010B UNTESTED RAW DIE: FAQ
  • +DS1181LE+: FAQ
  • DS1225AB-150: FAQ
  • +DS1225AB-150IND+: FAQ
  • +DS1225AD-200IND: FAQ
  • +DS1230Y-70IND+: FAQ
  • +DS1230Y: FAQ
  • +DS1235A: FAQ
  • +DS1236 UNTESTED UNLASERED DIE: FAQ
  • +DS1267-010: FAQ
  • +DS1267-10 UNTESTED RAW DIE: FAQ
  • +DS1270Y-70#: FAQ
  • +DS1270Y-70IND#: FAQ
  • +DS1312+: FAQ
  • +DS1402 BUTTON TO RJ11 PLUG CABLE: FAQ
  • +DS1402-RP8+: FAQ
  • +DS1402D-DR8+: FAQ
  • +DS1410E: FAQ
  • +DS1644-120: FAQ
  • +DS1669N-010: FAQ
  • +DS1821C+: FAQ
  • +DS1856B-020+: FAQ
  • +DS1856M: FAQ
  • +DS1859: FAQ
  • +DS1875K#: FAQ
  • +DS1904L-F5#: FAQ
  • +DS1920-F5+: FAQ
  • +DS1921: FAQ
  • +DS1922: FAQ
  • +DS1954: FAQ
  • +DS1961S: FAQ
  • +DS1963S: FAQ
  • +DS1971-F5+: FAQ
  • +DS1973-F3+: FAQ
  • +DS1977-F5#: FAQ
  • +DS1990A-019-F5A#CB: FAQ
  • +DS1990A-F3+: FAQ
  • +DS1990A-F5+: FAQ
  • +DS1991: FAQ
  • +DS1993: FAQ
  • +DS21554: FAQ
  • +DS2155DK: FAQ
  • +DS2155LNC2+: FAQ
  • +DS2482S-100+: FAQ
  • DS2482S-800+T&R: FAQ
  • +DS2483: FAQ
  • DS2490: FAQ
  • +DS2490S+: FAQ
  • +DS2506: FAQ
  • +DS26502DK: FAQ
  • +DS26502L+: FAQ
  • +DS26504: FAQ
  • +DS26504L+: FAQ
  • DS26514: FAQ
  • +DS26514GN+: FAQ
  • +DS26518DK: FAQ
  • +DS26518G+: FAQ
  • +DS26518GN+: FAQ
  • +DS26521L+: FAQ
  • +DS28CN01: FAQ
  • +DS28E01: FAQ
  • +DS28E04S-100+: FAQ
  • +DS28E11P+: FAQ
  • +DS3150TN+: FAQ
  • +DS3177+: FAQ
  • +DS34S132: FAQ
  • +DS34T101GN+: FAQ
  • +DS34T104: FAQ
  • +DS34T108GN+: FAQ
  • +DS3911: FAQ
  • +DS3935VGTL+: FAQ
  • +DS4100H+: FAQ
  • +DS4125: FAQ
  • DS4830A: FAQ
  • +DS4830AEVKIT: FAQ
  • +DS4830AT+: FAQ
  • DS75S-C1+T&R: FAQ
  • +DS80C320: FAQ
  • +DS80C323-ECD+: FAQ
  • +DS80C400-KIT: FAQ
  • +DS89C430-ENL+: FAQ
  • DS89C430: FAQ
  • +DS89C450-ENG+: FAQ
  • +DS89C450-QNG+: FAQ
  • +DS9034PC+: FAQ
  • +DS9034PCX+: FAQ
  • +DS9072: FAQ
  • +DS9090EVKIT#: FAQ
  • +DS9092+: FAQ
  • +DS9092L+: FAQ
  • +DS9092L: FAQ
  • +DS9093S+: FAQ
  • +DS9097U-009#: FAQ
  • +DS9097U-E25: FAQ
  • +DS9097U-S09#: FAQ
  • +DS9107+: FAQ
  • +DS9120P+: FAQ
  • +DS91230: FAQ
  • +DS9481P-300#: FAQ
  • +DS9490B#: FAQ
  • +DS9490B: FAQ
  • +DS9490R#: FAQ
  • +DSQ2FL1-J00+T: FAQ
  • +EV1HMC994APM5: FAQ
  • +EVAL-CN0566-RPIZ: FAQ
  • +EVAL-HCRWATCH4Z: FAQ
  • +EVAL-PRAOPAMP: FAQ
  • HMC-T2100: FAQ
  • +HMC1087: FAQ
  • +HMC1114: FAQ
  • +HMC342G: FAQ
  • +HMC518: FAQ
  • +HMC590: FAQ
  • +HMC6000: FAQ
  • +HMC605LP3E: FAQ
  • +HMC624: FAQ
  • +HMC6300G: FAQ
  • +HMC757: FAQ
  • +HMC852: FAQ
  • +HMC874: FAQ
  • +HMC930A: FAQ
  • +HMC994A: FAQ
  • +HSC-ADC-EVALB-DC: FAQ
  • HSC-ADC-EVALC: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +HSC_EVALBOARD: FAQ
  • +IA188EBPLC84IR2: FAQ
  • +IC0400C778BF+LTB: FAQ
  • +LM75BIMM-3+: FAQ
  • +LT1017: FAQ
  • +LT1161: FAQ
  • +LT1640A: FAQ
  • +LT4256-2: FAQ
  • +LT4293: FAQ
  • +LT4322: FAQ
  • +LTC2937: FAQ
  • +LTC2954: FAQ
  • +LTC2984: FAQ
  • +LTC2992: FAQ
  • +LTC3310: FAQ
  • +LTC4162: FAQ
  • +LTC4231: FAQ
  • +LTC4267-1: FAQ
  • +LTC4286: FAQ
  • +LTC4292: FAQ
  • +LTC4359: FAQ
  • +LTC4364: FAQ
  • +LTC4366: FAQ
  • +LTC4370: FAQ
  • +LTC4418: FAQ
  • +LTC4421: FAQ
  • +LTC6957-1: FAQ
  • +LTC7000: FAQ
  • +LTC9101-1: FAQ
  • +LTC9101-3: FAQ
  • +LTC9111: FAQ
  • +LTM2987: FAQ
  • +LTM4654: FAQ
  • +LTM4739: FAQ
  • +LTP5900-WHM: FAQ
  • +LTP5902-WHM: FAQ
  • +LTP8802: FAQ
  • +LTpowerCAD: FAQ
  • +LTSPICE: FAQ
  • +MAX-ECG-MONITOR: FAQ
  • +MAX-HEALTH-BAND: FAQ
  • +MAX-HEALTHBAND: FAQ
  • +MAX038CWP+_T1: FAQ
  • +MAX104CHC: FAQ
  • MAX13256: FAQ
  • +MAX13256ATB+: FAQ
  • +MAX14529E: FAQ
  • +MAX14626ETT+T: FAQ
  • +MAX14648: FAQ
  • MAX1464: FAQ
  • -MAX1464EVKIT: FAQ
    • Are there any programming examples available for the MAX1464?
    • Can I use the Control program in both 3-wire and 4-wire communication for the MAX1464?
    • Can I use the MAX1464 hardware debugger program in both 3-wire and 4-wire communication?
    • Can Partition-1 (user portion) of the MAX1464 flash memory be accessed by the CPU program?
    • Can the MAX1464 be used to measure the RTDs or K-type thermocouples?
    • Can the op amps on the MAX1464 be used as uncommitted op amps?
    • Can the second-order compensation algorithm built into the MAX1464 Control Program be used for real compensation in production?
    • Does the input impedance of the MAX1464 change with different PGA gain settings? How?
    • How can I switch the MAX1464 EV board from 3-wire to 4-wire communication, and vice versa?
    • How can the Control Program be used for the MAX1464?
    • How can the MAX1464 Hardware Debugger be used?
    • How do I program the MAX1464?
    • How is the conversion resolution affected by the changing conversion rate in the MAX1464?
    • How many input channels does the MAX1464 have?
    • I get 'file operation' failure error when launching the Control Program for the MAX1464. What is the problem?
    • Is it possible to call the MAX1464 DLL functions from Visual Basic?
    • Is the common-mode range specification the same for all PGA gain settings in the MAX1464?
    • Is the internal temperature sensor of the MAX1463 the same as on the MAX1464?
    • Is the MAX1464 temperature sensor output ratiometric to VDD?
    • MAX1464EVKIT Software OS Support
    • My setup is correct but cannot communicate with the MAX1464. What is the problem?
    • On what platform are the MAX1464 DLLs developed?
    • The 'DUT?' button on the Control Program window does not turn green when I start the program for the MAX1464. What is wrong?
    • Turning the potentiometers on the EV board does not change the input to the MAX1464. What is the problem?
    • What are the differences between 3-wire and 4-wire interfaces for the MAX1464?
    • What are the hardware differences between the MAX1463 and the MAX1464?
    • What are the register definition differences between MAX1463 and MAX1464?
    • What are the trade-offs between power consumption and conversion speed in the MAX1464?
    • What extent of programming can be realized with the available 4kB of flash memory for the MAX1464?
    • What input voltage range can the MAX1464 accommodate?
    • What instructions are available for the MAX1464 microprocessor?
    • What is an example application of the MAX1464 signal conditioner?
    • What is included in the MAX1464 evaluation kit?
    • What is the allowed common-mode voltage range for the INPx and INMx input voltages in the MAX1464?
    • What is the flash-memory capacity in the MAX1464?
    • What is the function of the partition-1 of the flash memory in the MAX1464?
    • What is the MAX1464's data-retention rating as a function of temperature?
    • What is the MAX1464?
    • What is the maximum supply voltage at which the MAX1464 can operate without damaging the part?
    • What is the relationship between ADC clock rates and power consumption in the MAX1464?
    • What is the sequence of events that take place to complete one ADC conversion for the MAX1464?
    • What should be the relationship between the output impedance of the sensor and input impedance of the MAX1464? How are they affecting each other?
    • What software tools are available to use with the MAX1464?
    • When starting an ADC cycle in the MAX1464, how long does it take before sampling starts?
    • When the MAX1464 ADC is sampling does it start with LSB or MSB?
    • With which Windows®︎ platform is the MAX1464 Hardware Debugger compatible?
    • With which Windows®︎ platforms are the MAX1464 DLLs compatible?
  • +MAX14655: FAQ
  • +MAX14672ETB+: FAQ
  • +MAX14699EWC+: FAQ
  • +MAX14713EWL+: FAQ
  • +MAX14714EWL+: FAQ
  • +MAX14721ATP+: FAQ
  • +MAX14723ATP+: FAQ
  • MAX1472: FAQ
  • +MAX1472AKA+T: FAQ
  • +MAX14738EWT+T: FAQ
  • +MAX1479ATE+: FAQ
  • MAX14870: FAQ
  • +MAX14870ETC+: FAQ
  • +MAX14871EVKIT#: FAQ
  • MAX14874: FAQ
  • +MAX14874ETC+: FAQ
  • +MAX15068ATP+: FAQ
  • +MAX15090BEWI+: FAQ
  • +MAX15096AEWE+T: FAQ
  • MAX15096AGWE+: FAQ
  • +MAX15096AGWE+T: FAQ
  • +MAX15162AATE+: FAQ
  • +MAX15162AATG+: FAQ
  • +MAX15500: FAQ
  • +MAX16025TE+: FAQ
  • +MAX16028TP+: FAQ
  • +MAX16029: FAQ
  • MAX16046: FAQ
  • +MAX16046ACB+: FAQ
  • +MAX16046EVKIT+: FAQ
  • +MAX16050ETI+: FAQ
  • +MAX16065: FAQ
  • +MAX16084_XS22B+_A1: FAQ
  • +MAX16122AWT+: FAQ
  • +MAX16126TCA/V+: FAQ
  • +MAX16126_TCA/V+_A1: FAQ
  • +MAX16127TC/V+: FAQ
  • MAX16141/V+: FAQ
  • +MAX16141/V+T: FAQ
  • MAX16141AAAF/VY+: FAQ
  • +MAX16141AAAF/VY+T: FAQ
  • +MAX16141ATD+: FAQ
  • +MAX16141EVKIT#: FAQ
  • +MAX16141_AAF/V+_A1: FAQ
  • +MAX16165: FAQ
  • +MAX16545BGPF+T: FAQ
  • +MAX16550AGPN+: FAQ
  • +MAX16550GPN+T: FAQ
  • MAX16602GGN+: FAQ
  • +MAX16602GGN+T: FAQ
  • +MAX16946: FAQ
  • +MAX17523ATE+: FAQ
  • +MAX17525ATP+: FAQ
  • +MAX17526AATP+: FAQ
  • +MAX17561AUD+: FAQ
  • +MAX17563AUD+: FAQ
  • +MAX17600ASA+: FAQ
  • +MAX17601ASA+: FAQ
  • +MAX17606: FAQ
  • MAX17608: FAQ
  • +MAX17608ATC+: FAQ
  • +MAX17609: FAQ
  • +MAX17612AATB+: FAQ
  • +MAX17613AATP+: FAQ
  • +MAX17613A_TP+_A1: FAQ
  • +MAX17613BATP+: FAQ
  • +MAX17616A: FAQ
  • +MAX20323AENC+: FAQ
  • +MAX20323CENC+T: FAQ
  • +MAX20323DENC+T: FAQ
  • +MAX20328AEWA+: FAQ
  • +MAX20330AEWA+: FAQ
  • +MAX20331AEWL+: FAQ
  • +MAX21000+TWCHS: FAQ
  • +MAX21001/V+: FAQ
  • +MAX2150ETI+: FAQ
  • +MAX22200ETJ+: FAQ
  • +MAX22201: FAQ
  • +MAX22256: FAQ
  • +MAX2242: FAQ
  • +MAX235CPG+G36: FAQ
  • +MAX235MDG/HR: FAQ
  • +MAX253ESA+: FAQ
  • MAX256: FAQ
  • +MAX256ASA+: FAQ
  • +MAX2654EXT+: FAQ
  • +MAX274A: FAQ
  • +MAX274EVKIT-DIP+: FAQ
  • MAX28200EWC+T: FAQ
  • +MAX28200EWC+TC02: FAQ
  • MAX2828: FAQ
  • MAX2828ETN+: FAQ
  • +MAX2828ETN+T: FAQ
  • +MAX2829ETN+: FAQ
  • MAX2830: FAQ
  • MAX2830ETM+: FAQ
  • +MAX2830ETM+T: FAQ
  • MAX2831: FAQ
  • +MAX2831EVKIT: FAQ
  • +MAX2837ETM+: FAQ
  • +MAX2837EVKIT+: FAQ
  • +MAX2850: FAQ
  • +MAX2851ITK+: FAQ
  • +MAX2900ETI+: FAQ
  • +MAX291: FAQ
  • +MAX2990ECB+: FAQ
  • +MAX2992: FAQ
  • +MAX3111ECWI: FAQ
  • +MAX31740ATA+: FAQ
  • MAX31760AEE+: FAQ
  • +MAX31760AEE+T: FAQ
  • +MAX31785: FAQ
  • +MAX31785AETL+T: FAQ
  • MAX31790: FAQ
  • +MAX31790ATI+T: FAQ
  • +MAX31856MUD+: FAQ
  • +MAX32510: FAQ
  • +MAX32520/W+JU: FAQ
  • +MAX32520ATJJ/V+: FAQ
  • +MAX32550: FAQ
  • +MAX32552-LCJ+: FAQ
  • MAX32552: FAQ
  • +MAX32555/B+: FAQ
  • MAX32555: FAQ
  • +MAX32558: FAQ
  • +MAX32560: FAQ
  • +MAX32590-LNS+: FAQ
  • +MAX32620-EVKIT#: FAQ
  • +MAX32620-EVKIT: FAQ
  • +MAX32620FTHR#: FAQ
  • MAX32620FTHR: FAQ
  • +MAX32620ICQ+: FAQ
  • +MAX32620IWG+T: FAQ
  • +MAX32621-EVKIT#: FAQ
  • +MAX32621IWG+T: FAQ
  • +MAX32625-EVKIT#: FAQ
  • +MAX32625-EVKIT: FAQ
  • MAX32625: FAQ
  • +MAX32625ITK+: FAQ
  • +MAX32625MBED#: FAQ
  • +MAX32625MBED: FAQ
  • +MAX32625NEXPAQ: FAQ
  • +MAX32625PICO#: FAQ
  • +MAX32626-EVKIT#: FAQ
  • +MAX32626-EVKIT: FAQ
  • +MAX32626: FAQ
  • +MAX32630-EVKIT#: FAQ
  • +MAX32630FTHR#: FAQ
  • MAX32630FTHR: FAQ
  • +MAX32630ICQ+: FAQ
  • MAX32630IWG+: FAQ
  • +MAX32630IWG+T: FAQ
  • +MAX32631-EVKIT#: FAQ
  • MAX32631: FAQ
  • +MAX32631ICQ+: FAQ
  • +MAX32632: FAQ
  • +MAX32650-EVKIT#: FAQ
  • +MAX32650EVKIT: FAQ
  • +MAX32650GCE+: FAQ
  • +MAX32650GWQ+T: FAQ
  • MAX32651: FAQ
  • +MAX32651GCE+: FAQ
  • +MAX32652: FAQ
  • +MAX32655GWY+: FAQ
  • +MAX32660-EVKIT#: FAQ
  • +MAX32660-EVSYS#: FAQ
  • MAX32660: FAQ
  • +MAX32660EVKIT: FAQ
  • +MAX32660GTG+T: FAQ
  • +MAX32660GTGBL+: FAQ
  • +MAX32660GTGLA+T: FAQ
  • +MAX32660GWE+: FAQ
  • +MAX32665EVKIT#: FAQ
  • +MAX32665GXMBT+T: FAQ
  • +MAX32666FTHR#: FAQ
  • +MAX32666GWP+: FAQ
  • MAX32666GWPBT+: FAQ
  • +MAX32666GWPBT+T: FAQ
  • +MAX32668GWPBL+: FAQ
  • +MAX32670GTL+: FAQ
  • +MAX3421: FAQ
  • +MAX34440ETLA1+: FAQ
  • +MAX34446ETL+T: FAQ
  • +MAX34451ETNA1+: FAQ
  • +MAX34451ETNA2+: FAQ
  • +MAX34451ETNA3+: FAQ
  • +MAX34461AA00+: FAQ
  • +MAX34463EXQA3+: FAQ
  • +MAX3600: FAQ
  • +MAX3601GTL+: FAQ
  • +MAX3634: FAQ
  • +MAX3711: FAQ
  • +MAX3735AE/D: FAQ
  • +MAX3735AETG+: FAQ
  • +MAX3736ETE+: FAQ
  • +MAX3738: FAQ
  • +MAX3740AETG+: FAQ
  • MAX3740AETG: FAQ
  • +MAX3747AEUB+: FAQ
  • +MAX3748HETE+: FAQ
  • +MAX3761: FAQ
  • MAX3869EHJ+: FAQ
  • +MAX3869EHJ+T: FAQ
  • +MAX40056EVKIT#: FAQ
  • +MAX40200ANS+: FAQ
  • MAX40200AUK+: FAQ
  • +MAX40200AUK+T: FAQ
  • MAX40203ANS+: FAQ
  • +MAX40203ANS+T: FAQ
  • +MAX40213: FAQ
  • +MAX4137: FAQ
  • +MAX41460EVKIT: FAQ
  • +MAX41460GUB+: FAQ
  • +MAX41461GUB+T: FAQ
  • +MAX41463GUB+: FAQ
  • +MAX4201EUK+: FAQ
  • +MAX4207: FAQ
  • +MAX4222EEE+: FAQ
  • +MAX4311EEE+: FAQ
  • +MAX4370: FAQ
  • +MAX4383EEE+: FAQ
  • +MAX4427MJA/883B: FAQ
  • +MAX4428ESA+: FAQ
  • +MAX44299: FAQ
  • +MAX4444ESE/GG8: FAQ
  • +MAX4550EVKIT: FAQ
  • +MAX4820ETP+: FAQ
  • +MAX4821: FAQ
  • +MAX4896ATP+: FAQ
  • +MAX4915AELT+: FAQ
  • +MAX5048CAUT+: FAQ
  • +MAX5859EXW-D: FAQ
  • +MAX5902AAEUT+: FAQ
  • +MAX5903AAETT+: FAQ
  • +MAX5921FESA+: FAQ
  • +MAX5933AESA+: FAQ
  • +MAX5943AEEE+: FAQ
  • +MAX5947BESA: FAQ
  • +MAX5954AETX+: FAQ
  • +MAX5954LETX+: FAQ
  • +MAX5965A: FAQ
  • +MAX5969AETB+: FAQ
  • +MAX5969BETB+: FAQ
  • +MAX5969BEVKIT+: FAQ
  • +MAX5971AETI+: FAQ
  • +MAX5971BETI+: FAQ
  • +MAX5974AATE+T: FAQ
  • +MAX5974CETE+: FAQ
  • MAX5974D: FAQ
  • +MAX5974DATE+: FAQ
  • +MAX5974EETE+: FAQ
  • +MAX5977AETP+: FAQ
  • MAX5980: FAQ
  • +MAX5980AGTJ+: FAQ
  • +MAX5988A: FAQ
  • +MAX5991AETP+: FAQ
  • +MAX5995AATE+: FAQ
  • +MAX5995AETE+T: FAQ
  • +MAX5995BATE+: FAQ
  • +MAX5995CETE+: FAQ
  • +MAX6495: FAQ
  • +MAX6496ATA/V+: FAQ
  • +MAX6615AEE+: FAQ
  • +MAX6639FAEE: FAQ
  • +MAX6641: FAQ
  • +MAX6643LBBAEE+: FAQ
  • MAX6650: FAQ
  • +MAX6650EUB+: FAQ
  • +MAX6653AEE+: FAQ
  • +MAX6682MUA+T: FAQ
  • +MAX6684ESA+: FAQ
  • +MAX6816: FAQ
  • +MAX6839XSD2+: FAQ
  • +MAX6895AALT+: FAQ
  • +MAX6895AAZT/V+T: FAQ
  • +MAX7030HATJ+: FAQ
  • +MAX7032: FAQ
  • MAX7037: FAQ
  • +MAX7037EGL+T: FAQ
  • +MAX7037EVKIT#: FAQ
  • +MAX7461EUK+: FAQ
  • +MAX7474EAE+_T1: FAQ
  • +MAX77729XEWN+: FAQ
  • +MAX77823EWZ+: FAQ
  • +MAX77859AEWO+: FAQ
  • +MAX77932BEWO+: FAQ
  • +MAX77932EWO+T: FAQ
  • +MAX77972: FAQ
  • +MAX78000EXG+: FAQ
  • +MAX78000FTHR: FAQ
  • +MAX78700: FAQ
  • +MAX8535: FAQ
  • +MAX8790AETP+: FAQ
  • +MAX8804: FAQ
  • +MAX881: FAQ
  • +MAX8902: FAQ
  • +MAX8903: FAQ
  • +MAX9272: FAQ
  • +MAX9295AGTJ/V+: FAQ
  • +MAX9295EGTN/V+T: FAQ
  • +MAX9296AGTM/V+: FAQ
  • +MAX96716A: FAQ
  • +MAX96751: FAQ
  • +MAX96752: FAQ
  • +MAX96793: FAQ
  • +MAX98089ETN+: FAQ
  • +MAX98089EVKIT#WLP: FAQ
  • MAX98090: FAQ
  • +MAX98090AETL+T: FAQ
  • +MAX98090AEWJ+: FAQ
  • +MAX98090EVKIT#WLP: FAQ
  • +MAX98091: FAQ
  • +MAX98373: FAQ
  • +MAX9860ETG+: FAQ
  • MAX9867: FAQ
  • +MAX9867ETJ+: FAQ
  • +MAX9867EVKIT+: FAQ
  • MAX9880A: FAQ
  • +MAX9880AETM+: FAQ
  • +MAX9880AEVKIT#: FAQ
  • +MAX9947ETE+: FAQ
  • +MAXADCLITE+: FAQ
  • +MAXCOAX2STP-HSD#: FAQ
  • +MAXPOWERTOOL002#: FAQ
  • +MAXQ1741: FAQ
  • +MAXQ1743: FAQ
  • +MAXQ1744-DNS+: FAQ
  • +MAXQ617: FAQ
  • MAXQ7667: FAQ
  • +MAXQ7667AACM/V+: FAQ
  • +MAXQUSBJTAGOW-KIT#: FAQ
  • +MAXREFDES100#: FAQ
  • +MAXREFDES101 SOFTWARE FOR WINDOWS 10: FAQ
  • +MAXREFDES101#: FAQ
  • +MAXREFDES103#: FAQ
  • +MAXREFDES104#: FAQ
  • +MAXREFDES105#: FAQ
  • +MAXREFDES106: FAQ
  • +MAXREFDES117#: FAQ
  • +MAXREFDES132#: FAQ
  • +MAXREFDES145#: FAQ
  • +MAXREFDES150#: FAQ
  • +MAXREFDES16#: FAQ
  • +MAXREFDES165#: FAQ
  • +MAXREFDES212#: FAQ
  • +MAXREFDES220#: FAQ
  • +MAXREFDES280: FAQ
  • +MAXREFDES31#: FAQ
  • +MAXREFDES37#: FAQ
  • +MAXREFDES4#: FAQ
  • +MAXREFDES42#: FAQ
  • +MAXREFDES70#: FAQ
  • +MAXREFDES73#: FAQ
  • +MAXREFDES74#: FAQ
  • MAXREFDES74: FAQ
  • +MAXREFDES77#: FAQ
  • +MAXREFDES79#: FAQ
  • +MINIQUSB: FAQ
  • +NO PART NUMBER: FAQ
  • +NONE: FAQ
  • +OP07: FAQ
  • +OP27: FAQ
  • +OP37: FAQ
  • +OP90: FAQ
  • +PCB, MAX2850EVKIT+: FAQ
  • PD-1370: FAQ
  • +PD20-1-1210: FAQ
  • +PD28-3-1021-TMCL: FAQ
  • +PD42-1-1140-TMCL: FAQ
  • +PD42-1-1243-IOLINK: FAQ
  • +PD42-1-1370-TMCL: FAQ
  • +PD42-4-1370-TMCL: FAQ
  • +PD57-1-1076: FAQ
  • +PD57-1-1160-TMCL: FAQ
  • +PD57-1-1260-TMCL: FAQ
  • +PD57-1-1378-CANOPEN: FAQ
  • +PD57-2-1160-TMCL: FAQ
  • +PD60-3-1260-TMCL: FAQ
  • +PH-MODULES-TRINAMIC: FAQ
  • +QBL4208-100-04-025: FAQ
  • +QBL4208-41-04-006: FAQ
  • +QBL4208-61-04-013: FAQ
  • +QBL5704-116-04-042: FAQ
  • +QSH2818-32-07-006: FAQ
  • +QSH4218-41-10-035: FAQ
  • +REF02A: FAQ
  • +RS485: FAQ
  • +SC-USB-SPI: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2602: FAQ
  • +SSM2603: FAQ
  • +STM1E-SFP02: FAQ
  • +STM1E-SFP22: FAQ
  • +SW02: FAQ
  • +TEST: FAQ
  • +TMC USB-2-485: FAQ
  • +TMC2041-EVAL: FAQ
  • +TMC2041-LA: FAQ
  • +TMC2130-LA: FAQ
  • +TMC2208SILENTSTEPSTICK: FAQ
  • +TMC2209 SILENTSTEPSTICK: FAQ
  • +TMC2209-LA-T: FAQ
  • +TMC2226-BOB: FAQ
  • +TMC2240: FAQ
  • +TMC2590: FAQ
  • +TMC262C-LA: FAQ
  • +TMC2660C-PA-T: FAQ
  • TMC2660C-PA: FAQ
  • +TMC429-I: FAQ
  • +TMC4361A-LA: FAQ
  • +TMC457: FAQ
  • +TMC4671: FAQ
  • +TMC5031: FAQ
  • +TMC5041-LA: FAQ
  • +TMC5062-LA: FAQ
  • +TMC5072-LA: FAQ
  • +TMC5130-EVAL-KIT: FAQ
  • +TMC5130A-TA: FAQ
  • +TMC5160 SILENTSTEPSTICK: FAQ
  • +TMC5160-BOB: FAQ
  • +TMC5160-EVAL: FAQ
  • +TMC5160A-TA: FAQ
  • +TMC5240: FAQ
  • +TMC5272-EVAL-KIT: FAQ
  • +TMC6140-EVAL: FAQ
  • +TMC8462: FAQ
  • +TMCM-1043: FAQ
  • +TMCM-1070: FAQ
  • +TMCM-110-42-485: FAQ
  • +TMCM-1110 STEPROCKER: FAQ
  • +TMCM-1140-TMCL: FAQ
  • +TMCM-1160-TMCL: FAQ
  • +TMCM-1180-TMCL: FAQ
  • +TMCM-1240: FAQ
  • +TMCM-1260-CANOPEN: FAQ
  • +TMCM-1260-TMCL: FAQ
  • +TMCM-1270-CANOPEN: FAQ
  • +TMCM-1290: FAQ
  • +TMCM-142-IF-TMCL: FAQ
  • +TMCM-1630-2C: FAQ
  • +TMCM-1630-4U: FAQ
  • +TMCM-1633-CANOPEN: FAQ
  • +TMCM-1636-24V-CANOPEN: FAQ
  • +TMCM-1640: FAQ
  • +TMCM-1690: FAQ
  • +TMCM-310/SG: FAQ
  • +TMCM-3110-TMCL: FAQ
  • +TMCM-3212-TMCL: FAQ
  • +TMCM-3230-TMCL: FAQ
  • +TMCM-3314: FAQ
  • +TMCM-3351-TMCL: FAQ
  • +TMCM-6110: FAQ
  • +TMCM-6212-TMCL: FAQ
  • +TMCM-6214-CANOPEN: FAQ
  • +TMCM-6214-TMCL: FAQ
  • +TMCS: FAQ
  • +TRINAMIC MISC SERVICE: FAQ
  • +TRINAMIC PACKAGING SURCHARGE: FAQ
  • +USB-2-RTMI: FAQ
  • +USB2GPIO#: FAQ
  • +USB2PMB2#: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VISUALAUDIO: FAQ
  • +VT202: FAQ
  • +VT273SAFQ: FAQ
  • What does the "C01" denote in DS75S-C01+?
  • What should I do with unused I/O pins on the DS2482S?
  • +ZLP32300: FAQ
  • +_DS9093A: FAQ

Turning the potentiometers on the EV board does not change the input to the MAX1464. What is the problem?

Two likely reasons are: 1) The jumpers JU11 and JU12 are not installed. 2) The potentiometers are not good. This is a less likely possibility. The integrity of the potentiometers can be checked by performing an ohmic measurement at the potentiometer's terminals.
Tags: MAX1464 000095274 8052 Core Products Precision Microcontrollers