Hello,
The AD74413R datasheet indicates that the input range in voltage input mode is 0 V to 10 V. If I want to increase that range to 0 V to 24 V, could I use a resistive voltage divider on SENSEH_x, SENSEHF_x, SENSEL_x, and SENSELF_x to increase it (see attached image)? This will also affect the current measurement path in current input/output mode, right?
Thank you very much in advance.