AD74413R
Recommended for New Designs
The AD74413R is a quad-channel software configurable input/output solution for building and process control applications. The AD74413R contains functionality...
Datasheet
AD74413R on Analog.com
Hello,
the AD74413R datasheet says that AVDD to AGND voltage must be between -0.3V and +30V. Is that +30 V upper limit the maximum peak voltage or can the AD74413R withstand higher voltage transients for short periods of time?
Thank you very much in advance.
Hi rafaelsf ,
thank you for your question, I will be happy to clarify the same.
As described in the text below "Table 12." in "Absolute Maximum Ratings" section +30V from AVDD to AGND is absolute maximum limit. Even short-term peak or transient may cause permanent damage to the chip. These limits should be considered as "maximum upper limits" - Absolute Maximum Ratings.
Let me know, if this gives you clarity concerning the same.
Note that operating voltage is lower AVDD = 14 V to 28.8 V (as per specification tables.)
Regards,
Arnost
Hi APavlik,
Thank you very much for your reply.
Yes, I assumed that the +30 V was the maximum voltage, but then I checked the schematic of the EVAL-AD74413R-DIOZ and it has a +/- 36 V TVS diode on the 24 V input (where AVDD is connected). That made me think that maybe the ADR7413 could withstand transient voltages above 30 V for a short period of time.
Hi rafaelsf ,
that is valid point, +24V TVS rating at EVAL-AD74413R-DIOZ is not ideal from AD74413R perspective. Thank you for bringing that to my attention.
We cannot guarantee any voltages higher than 30V on AVDD and Datasheet is ultimate source of information. Part may/may not survive particular transients, however there is no guarantee, even more I would say there is risk of permanent damage or impact on the chip performance.
Regards,
Arnost