Post Go back to editing

Calculate the actual measured capacitance value

Category: Software
Product Number: AD7142

I would like to know whether it is possible to calculate the actual measured capacitance value (in pF) from the AD7142 or AD7147, for example by using the offset and the readings from the AD7142/AD7147. Is there a formula that can be used for this calculation?

Parents
  • Hi  ,

    While it is possible to calculate the absolute capacitance value, it will not be very accurate, a rough estimate could be gained by summing the Offset value and the CDC result value, the Offset resolution is 0.32pF, the CDC result resolution is 0.244fF.

    Multiplying the offset and CDC result codes by the resolution values and adding them together will give the rough estimate. Greater accuracy could be achieved by at least calibrating the zero capacitance value and also at a known capacitance value.

    For example if at the zero capacitance value, Offset = 17 and CDC Result = 2224, each code change in offset adds 0.32pF (The offset value must be incremented when the CDC Result is close to saturation) and each code change in CDC Result adds 0.244fF.

    So if a measurement gives the result, Offset = 25 and CDC Result = 40,000, the measured capacitance is (25-17)*0.32pF + (40,000 - 2224)*0.244fF = 11.78pF

    Regards,

    Maurice.

Reply
  • Hi  ,

    While it is possible to calculate the absolute capacitance value, it will not be very accurate, a rough estimate could be gained by summing the Offset value and the CDC result value, the Offset resolution is 0.32pF, the CDC result resolution is 0.244fF.

    Multiplying the offset and CDC result codes by the resolution values and adding them together will give the rough estimate. Greater accuracy could be achieved by at least calibrating the zero capacitance value and also at a known capacitance value.

    For example if at the zero capacitance value, Offset = 17 and CDC Result = 2224, each code change in offset adds 0.32pF (The offset value must be incremented when the CDC Result is close to saturation) and each code change in CDC Result adds 0.244fF.

    So if a measurement gives the result, Offset = 25 and CDC Result = 40,000, the measured capacitance is (25-17)*0.32pF + (40,000 - 2224)*0.244fF = 11.78pF

    Regards,

    Maurice.

Children
No Data