- I would like to adjust the sensitivity of the AD7147, for example, to increase or decrease the CDC output corresponding to 1pF. Is there a method to achieve this?
- How can I convert the CDC output into capacitance?
AD7147
Production
The AD7147 CapTouch™ controller is designed for use with capacitance sensors implementing functions such as buttons, scroll bars, and wheels. The sensors...
Datasheet
AD7147 on Analog.com
AD7147A
Obsolete
The AD7147A CapTouch™ controller is designed for use with capacitance sensors implementing functions such as buttons, scroll bars, and wheels. The sensors...
Datasheet
AD7147A on Analog.com
Hi HuaWuque,
It is not possible to change the sensitivity, the input range is fixed at +/- 8pF, the CDC is 16-bit resolution so each count has a weight of 16pF/65536 = 244 aF.
If an offset capacitance is configured this should be added to the total capacitance value at 0.32pF per count
Regards,
Maurice.
Hi HuaWuque,
It is not possible to change the sensitivity, the input range is fixed at +/- 8pF, the CDC is 16-bit resolution so each count has a weight of 16pF/65536 = 244 aF.
If an offset capacitance is configured this should be added to the total capacitance value at 0.32pF per count
Regards,
Maurice.