Post Go back to editing

Values of PID controller resistor and capacitor

Category: Datasheet/Specs
Product Number: ADN8835

I desire to control TEC of a butterfly 14 pin laser with ADN8835 in analog feedback mode. But I am facing issue in determining the values for resistors and capacitors connected between IN1N, IN2N, IN1P, IN2P, OUT1 and OUT2. The laser i am using is Thorlabs SFL1550P, whose TEC voltage at 25celcius is 0.6V and current is 0.3A. I want to maintain temperature at 25 Celcius. I calculated compensated thermistor resistance Rx using Tlow=0, Tmid=25, Thigh=50. Please help me with the required values.