Hello,
I’m trying to use the AD734 as a ‘Lock in’ amplifier.
I have the AD734 on a breadboard connected as in fig. 24 page 20 of the datasheet (basic multiplier circuit).
The denominator is set to 1V with the resistors specified in table 5 page 20 of the datasheet.
X1 input is a sine wave with an amplitude of 300mV (600mV p-p) and a frequency of 350 KHz.
X2 is grounded.
Y1 input is a square wave with an amplitude of 1V (2V p-p) and the frequency of 350 KHz.
Y2 is grounded.
At the output I have a the fully rectified sine wave but small spikes appears (FIG. 1 below) at half the frequency (350KHz /2).

fig.1
If the amplitude of the square wave is increased to just 3V p-p the spikes exponentially increases (fig.2 and 3).

fig.2

fig.3
I can’t get rid of them.
Any suggestion?
Thanks