Post Go back to editing

Sample rate of the MAX86150 is not accurate

Category: Hardware
Product Number: MAX86150

I am recording data with MAX86150, the sample rate is set to 200sps for ECG and PPG. but when I record the data for each IC the sample rate is a number near 200 and it is not accurate.

this is the result:

recording time = 24:29:06 (HH:MM:SS) = 88146s 

the desired samples based on the recording time = 88146 x 200 = 17629200 samples

but total samples generated by MAX86150 = 17645525 samples

real sample rate = 17,645,525 / 88,146 = 200.185 sample per second

this test with another MAX86150 IC results 199.45sps. 

Has anyone else faced this problem? and is there any solution to solve this problem?

Parents Reply Children
No Data