Post Go back to editing

LT5400 Data Interpretation

Category: Datasheet/Specs
Product Number: LT5400

I hope this finds you well. Our team is using the LT5400 quad resistor network in one of our designs and we are hoping you can clarify some technical details for us. 

 
We are intending to use the LT5400 quad resistor in a circuit that is to maintain a very tight accuracy specification. Our Electrical Engineering team has identified the resistor as being the main contributor to the accuracy drift of our signal chains. As such, understanding the specifications of the matching drift is very important to us. 
The first question we have is regarding the resistor matching over time plot in page 5 of the datasheet. Are you able to provide more details or explanation of the test conditions on how this drift was obtained? In addition, can you clarify what the different traces on the plot represent? Knowing the temperature this plot was obtained at would be especially helpful as we are considering replicating this plot using accelerated life testing. Any details on the test setup used to get this plot would also be appreciated. 

The second question is regarding the "Resistor Matching Ratio Long Term Drift"  specification on page 4 of the datasheet. Our team is interpreting the meaning for that particular field as: resistors exposed to the specified test conditions have a typical ppm value as specified."  Can you clarify if this is the correct interpretation of the field? 
 
Thank you very much for your help. 

Thread Notes

  • Hi  

    Thanks for taking an interest in LT5400. 

    The change in Matching vs Time plot in page 5 was tested for 2000 hours at 35°C and 10mW that was specified under electrical characteristics section. Also, the traces in the plot represents different units that was tested. 

    For your second question, yes, that is the correct interpretation. 

    I hope this information helps. 

    Thanks,

    Mae

  • I can add a bit more to what Mae has already contributed, with info from the original design manager for LT5400. The test conditions for the drift plot were obtained using the 4x10k variant, with pairs of resistors set up as a divider across +/-10V. The voltage in the middle was monitored and the equivalent change in matching was calculated in ppm for the curve. Each line in the curve is thus one pair of resistors. The curve below is for 35C as Mae stated.

    Regarding the last question, yes, you won't typically see values beyond the 2pmm tested. We didn't in our own lab testing.