Currently our company is using MAX96705 and MAX96706, we want to change the serializer to MAX96705a. However, there is no extra datasheet for max96705a. So what is the difference between max96705a and max96705? or there is no?
MAX96705
Production
The MAX96705 is a compact serializer with features especially suited for automotive camera applications. It is function and pin compatible with the MAX9271...
Datasheet
MAX96705 on Analog.com
MAX96705A
Production
The MAX96705A is a compact serializer with features especially suited for automotive camera applications. It is function and pin compatible with the MAX9271...
Datasheet
MAX96705A on Analog.com
MAX96706
Production
The MAX96706 is a compact deserializer especially suited for automotive camera applications. Features include adaptive equalization and an output crosspoint...
Datasheet
MAX96706 on Analog.com
Currently our company is using MAX96705 and MAX96706, we want to change the serializer to MAX96705a. However, there is no extra datasheet for max96705a. So what is the difference between max96705a and max96705? or there is no?
jnaso - Moved from Interface and Isolation to Other Products. Post date updated from Monday, January 8, 2024 7:58 AM UTC to Tuesday, January 9, 2024 9:23 PM UTC to reflect the move.