Post Go back to editing

How to connect the LTC1966 with an AC signal from sampling resistors centered to GND.

Category: Hardware
Product Number: LTC1966

So, i am working on a energy harvesting current meter and i want to use LTC1966 to get a decent DC representation of the RMS current. 

Since the CT is time multiplexed i am not able to DC bias it, actually the sampling resistor is split in two branches, centered around GND. 

So i wonder how i should connect the LTC1966, i understand that it must be DC biased on one side, so would it be as simple as DC isolating it from this sampling resistor and biasing to 1.65V (VCC/2) after this 100nF capacitor? or should i do differently?

Thread Notes