AD633
Production
The AD633 is a functionally complete, four-quadrant, analog multiplier. It includes high impedance, differential X and Y inputs, and a high impedance summing...
Datasheet
AD633 on Analog.com
Hi, AD633 datasheet contains optional offset trim configuration (figure 11, page 8). As a mean to nullify offsets on X, Y and W pins.
Unfortunately there is no procedure how to actually trim those offsets. Each of those offsets influences output.
How to trim it? What is the procedure?
I can't figure out it.
Hello Chupacabras,
AD633's accuracy is trimmed via laser-trim method. Figure 11 is used as compensation circuit to reduce nonlinearity errors on the input or output. its like a potentiometer that you can adjust depending on the offset that you are seeing that's why it was called a trim circuit.
Best Regards
Kenneth
Hi,
I believe that the question has already been answered so I am closing this thread. Thank you!
Regards,
Paul
Hi,
sorry for not responding. I figured out proper procedure on some other forum and I forgot to get back here.
This is the procedure:
1. set X=0V, Y=0V. and trim Z so the output is zero. (this results Z to be properly trimmed, because offsets on X and Y are negligible in this case)
2. set X=0V, Y=10V. and trim X so the output is zero. (this results X to be properly trimmed)
3. set X=10V, Y=0V. and trim Y so the output is zero. (this results Y to be properly trimmed)