In datasheet page 10,section "Output offset",at the end of first paragraph.


" When the surface mount package is used, all the unused pins should be grounded."
Does it mean those NC pins shoud be grounded?
Best Regards.
LTC1063
Production
The LTC1063 is the first monolithic filter providing both clock-tunability, low DC output offset and over 12-bit DC accuracy. The frequency response of...
Datasheet
LTC1063 on Analog.com
In datasheet page 10,section "Output offset",at the end of first paragraph.


" When the surface mount package is used, all the unused pins should be grounded."
Does it mean those NC pins shoud be grounded?
Best Regards.
Hello SavageZ ,
Yes. It seems like unused pins is pertaining to NC pins. Connecting them to ground should have no issue since "ideally", they have no internal/external function (please inform us if it does so we could check).
Regards,
Kenneth
Thank you,I will give a try!
Hi,
Assumed answered offline. If you still need assistance, please create a new thread.
Thanks,
Mae