Post Go back to editing

MAX14915 Driver IC channel issue

Product Number: MAX14915

Hi,

I am working on MAX14915 with Infineon controller through SPI interface. I have configured SPI in master mode with CPHA and CPOL is configured to zero. Taken transmit as MSB and made enable and SYNCH pin as high. By making the CS pin low writing first 8 bits as command and next 8 bits as data to SetOut Register.

The issue I am facing here is If i am trying to on the 8th switch, along with 8th switch 7th switch is also getting on. If I am trying to on the 5th switch the 4th switch is also getting on. If i am tying to on the specified channel then along with it the before channel is also getting on.

Could you please help me with on of a particular specified output channel??

Thanks 



Moved & added tags.
[edited by: emassa at 1:20 PM (GMT -4) on 19 Apr 2023]
Parents Reply Children
No Data