Post Go back to editing

How to use a power adapter with the MAX77860

Category: Hardware
Product Number: MAX77860

My battery charger design needs to accept power from USB or power adapter (power from a wall cube / power supply).  The MAX77860 datasheet claims its power input can accept power from USB or a number of chargers including a "dedicated charger" with current of 500mA to Imax.  Is a "dedicated charger" a standard power supply that has no communication capabilities with the mAX77860?  And, how does the MAX77860 know how much current to draw?

Thanks



Added Tag
[edited by: GenevaCooper at 10:22 PM (GMT -5) on 2 Feb 2023]
Parents Reply Children
No Data