Post Go back to editing

Charge 1S2P lithium with MAX77751

Category: Hardware
Product Number: MAX77751

Hello,

I am looking at the MAX77751 to manage charge of 2 Lithium cell in parallel (1S2P).

Batteries are 2450mA each so a total of 6800mAh.

Each recharge with a current of 1.475A

Some questions:

Can I place simply these 2 cells in parallel and use the MAX77751  ?

Do I need additional feature protection (temperature cell ?) ?

Any balancing to add ?

How can I ensure cells will be charged before 6 hours limits set by the MAX77751  ?

Many thanks in advance

Phil



Added Tag: LMXMprodsupport
[edited by: GenevaCooper at 6:44 PM (GMT -5) on 20 Jan 2023]