Post Go back to editing

MAX25239 & MAX25240 Performance

Product Number: MAX25239

Hello,

I am looking for a DC Back&Boost with an input [12V-35V] and 24V output. Power consumtion between [40W-90W].

According to the datasheet "The MAX25239/MAX25240 offers fixed output voltages and programmable output voltages in the range of 3V to
20V." Isn't it possible to make it work at 24V output? 

Have any body experienced it? Do you recommend any other IC?

Thank you in advance.



Added product number tag.
[edited by: emassa at 10:03 PM (GMT -5) on 5 Jan 2023]