I am using this ADA4522 as voltage follower which is supplied with +35V and -5V. When input signal with below specs is given the OpAmp is heating
Input signal specs:
20Vpk, 5us rise/fall time and 2us high/low time.
I am using this ADA4522 as voltage follower which is supplied with +35V and -5V. When input signal with below specs is given the OpAmp is heating
Input signal specs:
20Vpk, 5us rise/fall time and 2us high/low time.
Hi,
Just a couple of questions about your setup:
1. When you configured the ADA4522 in a voltage follower, is there a feedback resistor?
2. Is there a source resistance or input resistance connected to the non-inverting input? If so, what's the value?
Thanks,
Donnie
Hi Donnie,
Thanks for the reply
1. When you configured the ADA4522 in a voltage follower, is there a feedback resistor?
No there is no feedback resistor
2. Is there a source resistance or input resistance connected to the non-inverting input? If so, what's the value?
Yes we have connected 2 Ohm resistor
Thanks
Preetham