Hello,
I need to simulate ADCMP600 in LTSpice, but cannot find model of ADCMP600 either in LTSpice or a generic SPICE model on analog.com. Can someone please point me to this device's simulation model?
Thanks!
ADCMP600
Production
The ADCMP600, ADCMP601, and ADCMP602 are very fast comparators fabricated on Analog Devices’ proprietary XFCB2 process. These comparators are exceptionally...
Datasheet
ADCMP600 on Analog.com
Hello,
I need to simulate ADCMP600 in LTSpice, but cannot find model of ADCMP600 either in LTSpice or a generic SPICE model on analog.com. Can someone please point me to this device's simulation model?
Thanks!
Hi,
We'll take this offline and send you the beta model (unreleased).
I am also looking for the LTspice model for the ADCMP600 comparator
File sent offline
Hello, any updates on the availability of this model? I am also interested in running a simulation with it (in place of the LTC6752 I'm currently using) .
Thank you,
Jorge
Hello, I also would need the SPICE Model for the ADCMP600. Could you send me the model via email?
May I get this model, please?
* ADCMP601 SPICE Macro-model * 06/26 Draft * LPS APPS Engineering * * This is not the final version of ADCMP601 Spice model * * This model was created based on the HSPICE version of ADCMP601 by JAV on 6/25/2018 * The ADCMP601 HSPICE model was modified so it can be used in LT SPICE simulator * This Spice model still needs to be tested to gurantee that it matches the HSPICE version * * Node assignments * non-inverting input * | inverting input * | | latch/hysteresis * | | | positive supply * | | | | negative supply * | | | | | output pin * | | | | | | * | | | | | | * | | | | | | .SUBCKT ADCMP601 3 4 5 6 2 1 c0 17 0 5e-13 c1 19 0 2e-13 c2 3 0 2e-13 c3 4 0 2e-13 dp 2 6 DESD e0 18 0 VALUE = {LIMIT (4*V(17,0),0.3,-0.3)} e1 20 0 VALUE = {LIMIT (1*V(19,0),0.3,-0.3)} g0 6 2 0 22 1 io 12 13 dc 1e-06 iq 22 0 dc 0.002422 r0 17 0 700 r1 18 19 1000 r2 3 13 100 r3 4 11 100 r4 21 0 50 rd 3 4 1e7 rp 6 2 1e5 rt 22 0 1 tc=0.0005 t0 20 0 21 0 z0=50 td=1.370e-9 vo 11 12 dc 0.001 x1 4 2 6 ADCMP601_ESD x2 3 2 6 ADCMP601_ESD x3 5 2 6 ADCMP601_ESD x4 1 2 6 ADCMP601_ESD xb 12 13 14 15 16 2 6 ADCMP601_BIAS xh 17 2 5 6 ADCMP601_HYST xi 12 13 14 15 16 17 2 6 ADCMP601_INPUT xo 1 2 21 6 ADCMP601_OUTPUT xv 12 13 17 2 6 ADCMP601_DVOS .ENDS ADCMP601 * * Bias Current Generator * .SUBCKT ADCMP601_BIAS 12 13 14 15 16 2 6 d0 201 202 DSIM1 d1 201 203 DSIM1 d2 205 206 DSIM1 d3 202 204 DSIM1 d4 203 204 DSIM1 d5 207 208 DSIM1 e0 203 0 13 0 1 e1 202 0 12 0 1 e2 205 0 201 0 1 e3 208 0 204 0 1 e4 210 0 VALUE = {LIMIT (1*V(6,209),1.6,0.6)} e5 219 0 VALUE = {LIMIT (5*V(211,207),1,0)} g0 2 6 VALUE = {LIMIT (0.0015*V(212,213),0.003,0)} g1 15 0 VALUE = {LIMIT (0.001*V(212,213),0.002,0)} g2 16 0 VALUE = {LIMIT (0.001*V(214,215),0.002,0)} g3 16 0 VALUE = {LIMIT (-0.001*V(214,216),0,-0.0002)} g4 0 14 VALUE = {LIMIT (0.002*V(217,218),1e-4,0)} *I=(0+0*V(219,220))+(0+0.2*V(217,218)) g5 6 2 VALUE = {LIMIT (0.002*V(217,218),5e-05,0)} i0 0 201 dc 0.001 i1 204 0 dc 0.001 i5 206 0 dc 0.001 i6 0 207 dc 0.001 r0 206 218 1 r1 220 0 1 v0 209 0 dc 1.9 v1 211 0 dc 1.6 v2 217 210 dc 0.2 v3 212 207 dc 0.025 v4 213 0 dc 1.6 v5 214 207 dc 0.025 v6 215 0 dc 0.6 v7 216 0 dc 1.7 .ENDS * * CMRR and PSRR Offset Generator * .SUBCKT ADCMP601_DVOS 12 13 17 2 6 e0 302 0 13 0 1 e1 304 0 12 0 1 g0 17 0 VALUE = {LIMIT (1.71e-06 - 3.3e-07*V(303,0),3e-06,-1e-06)} *I = 1.71e-06 -3.3e-07*V(303,0) g1 17 0 VALUE = {LIMIT (6.667e-07*V(6,301),2e-06,0)} r0 302 303 1000 r1 303 304 1000 v0 301 2 dc 2.5 .ENDS * * ESD Diodes * .SUBCKT ADCMP601_ESD 601 602 606 d0 601 606 DESD d1 602 601 DESD .ENDS * * Hysteresis and Latch Function * .SUBCKT ADCMP601_HYST 17 2 5 6 c0 410 409 3.4e-11 c1 401 0 1e-12 d0 0 404 DSIM1 d1 401 5 DSIM3 e0 402 405 405 403 1 e1 412 0 VALUE = {LIMIT (20*V(17,0),0.3,-0.3)} f1 6 0 VALUE = {LIMIT (7*I(v1),0.0007,0)} f2 0 2 VALUE = {LIMIT (8*I(v2),0.0008,0)} g0 408 17 VALUE = {LIMIT (0.01*V(410,409),0.0003,-0.0003)} g1 411 0 VALUE = {LIMIT (0.01*V(414,0),3e-4,0)} h0 413 0 VALUE = {LIMIT (1000*I(v0),0.030,0)} i2 403 0 dc 0.00125 i3 5 0 dc 1.25e-06 i5 0 405 dc 1e-06 q0 410 0 411 0 NPN_IN1 q1 409 412 411 0 NPN_IN1 r0 403 404 1000 r1 402 401 7500 r3 408 410 100 r4 408 409 100 r5 414 0 50 t0 413 0 414 0 z0=50 td=7e-10 v0 406 405 0 v1 407 406 0 v2 0 407 0 v4 408 0 dc 1 .ENDS * * Input Stage * .SUBCKT ADCMP601_INPUT 12 13 14 15 16 17 2 6 e0 101 0 0 2 -1 e1 102 0 0 6 -1 g0 102 17 poly(3) 108 107 106 105 104 103 0 0.01 0.01 0.01 q0 103 13 14 0 PNP_IN1 q1 104 12 14 0 PNP_IN1 q2 105 13 15 0 NPN_IN1 q3 106 12 15 0 NPN_IN1 q4 107 13 16 0 NPN_IN2 q5 108 12 16 0 NPN_IN2 r0 101 103 200 r1 101 104 200 r2 102 105 90 r3 102 106 90 r4 102 107 80 r5 102 108 80 .ENDS * * Output Stage * .SUBCKT ADCMP601_OUTPUT 1 2 21 6 c0 1 507 8.8e-13 c2 505 504 6e-14 c3 503 504 6e-14 d0 504 503 DSIM2 d1 505 504 DSIM2 d2 506 505 DSIM1 d3 503 501 DSIM1 e0 506 2 508 0 1 e1 6 501 502 0 1 e2 507 0 6 2 0.5 g0 0 505 VALUE = {LIMIT (-0.0042667*V(21,0),0.00032,-0.00032)} g1 503 0 VALUE = {LIMIT (0.0042667*V(21,0),0.00032,-0.00032)} g2 6 0 VALUE = {LIMIT (-0.0085333*V(21,0),0.00064,0)} g3 0 2 VALUE = {LIMIT (0.0085333*V(21,0),0.00064,0)} i4 0 508 dc 0.001 i5 0 502 dc 0.001 q0 504 505 2 2 NPN_OUT q1 504 503 6 2 PNP_OUT r0 1 507 50000 r1 504 1 10 r3 508 0 850 tc=-0.00302 r4 502 0 850 tc=-0.00302 .ENDS * * Models Used * .model DESD d cjo=5e-14 is=1e-17 rs=0.5 eg=1.12 .model DSIM1 d is=1e-12 .model DSIM2 d is=1e-14 eg=0.950 .model DSIM3 d is=1e-15 .model NPN_IN1 npn bf=140 cjc=1.20e-14 cje=2.78e-14 is=9.1e-18 rb=60 re=400 tf=4.7e-12 .model NPN_IN2 npn bf=1e6 cjc=1.20e-14 cje=2.78e-14 is=9.1e-18 rb=60 re=400 tf=4.7e-12 .model PNP_IN1 pnp bf=25 cjc=5.50e-14 cje=1.05e-13 is=3.5e-17 rb=75 re=600 tf=1.2e-12 .model NPN_OUT npn bf=75 cjc=1.60e-13 cjs=6.5e-14 is=1.0e-16 vaf=50 .model PNP_OUT pnp bf=60 cjc=1.50e-13 cjs=6.5e-14 is=6.4e-17 vaf=30
what is your email address?
cshappee@markem-imaje.com