Post Go back to editing

ADCMP600 SPICE Model

Thread Summary

The user is seeking the LTSpice model for the ADCMP600 comparator, which is not available in LTSpice or on the Analog Devices website. The support engineer provided a beta model for ADCMP601, which can be used as a substitute. The model includes subcircuits for bias current, CMRR and PSRR offset, ESD diodes, hysteresis and latch, and the input and output stages. The user reported issues with the latching feature, but the support engineer suggested reaching out to ADI for further assistance. The model is specific to LTSpice and may not work in PSPICE due to syntax differences.
AI Generated Content

Hello, 

I need to simulate ADCMP600 in LTSpice, but cannot find model of ADCMP600 either in LTSpice or a generic SPICE model on analog.com. Can someone please point me to this device's simulation model?

Thanks!