ADCMP600
Production
The ADCMP600, ADCMP601, and ADCMP602 are very fast comparators fabricated on Analog Devices’ proprietary XFCB2 process. These comparators are exceptionally...
Datasheet
ADCMP600 on Analog.com
Hello,
I need to simulate ADCMP600 in LTSpice, but cannot find model of ADCMP600 either in LTSpice or a generic SPICE model on analog.com. Can someone please point me to this device's simulation model?
Thanks!
Hi,
We'll take this offline and send you the beta model (unreleased).
I am also looking for the LTspice model for the ADCMP600 comparator
File sent offline
Hello, any updates on the availability of this model? I am also interested in running a simulation with it (in place of the LTC6752 I'm currently using) .
Thank you,
Jorge
Hello, I also would need the SPICE Model for the ADCMP600. Could you send me the model via email?
May I get this model, please?
* ADCMP601 SPICE Macro-model * 06/26 Draft * LPS APPS Engineering * * This is not the final version of ADCMP601 Spice model * * This model was created based on the HSPICE version of ADCMP601 by JAV on 6/25/2018 * The ADCMP601 HSPICE model was modified so it can be used in LT SPICE simulator * This Spice model still needs to be tested to gurantee that it matches the HSPICE version * * Node assignments * non-inverting input * | inverting input * | | latch/hysteresis * | | | positive supply * | | | | negative supply * | | | | | output pin * | | | | | | * | | | | | | * | | | | | | .SUBCKT ADCMP601 3 4 5 6 2 1 c0 17 0 5e-13 c1 19 0 2e-13 c2 3 0 2e-13 c3 4 0 2e-13 dp 2 6 DESD e0 18 0 VALUE = {LIMIT (4*V(17,0),0.3,-0.3)} e1 20 0 VALUE = {LIMIT (1*V(19,0),0.3,-0.3)} g0 6 2 0 22 1 io 12 13 dc 1e-06 iq 22 0 dc 0.002422 r0 17 0 700 r1 18 19 1000 r2 3 13 100 r3 4 11 100 r4 21 0 50 rd 3 4 1e7 rp 6 2 1e5 rt 22 0 1 tc=0.0005 t0 20 0 21 0 z0=50 td=1.370e-9 vo 11 12 dc 0.001 x1 4 2 6 ADCMP601_ESD x2 3 2 6 ADCMP601_ESD x3 5 2 6 ADCMP601_ESD x4 1 2 6 ADCMP601_ESD xb 12 13 14 15 16 2 6 ADCMP601_BIAS xh 17 2 5 6 ADCMP601_HYST xi 12 13 14 15 16 17 2 6 ADCMP601_INPUT xo 1 2 21 6 ADCMP601_OUTPUT xv 12 13 17 2 6 ADCMP601_DVOS .ENDS ADCMP601 * * Bias Current Generator * .SUBCKT ADCMP601_BIAS 12 13 14 15 16 2 6 d0 201 202 DSIM1 d1 201 203 DSIM1 d2 205 206 DSIM1 d3 202 204 DSIM1 d4 203 204 DSIM1 d5 207 208 DSIM1 e0 203 0 13 0 1 e1 202 0 12 0 1 e2 205 0 201 0 1 e3 208 0 204 0 1 e4 210 0 VALUE = {LIMIT (1*V(6,209),1.6,0.6)} e5 219 0 VALUE = {LIMIT (5*V(211,207),1,0)} g0 2 6 VALUE = {LIMIT (0.0015*V(212,213),0.003,0)} g1 15 0 VALUE = {LIMIT (0.001*V(212,213),0.002,0)} g2 16 0 VALUE = {LIMIT (0.001*V(214,215),0.002,0)} g3 16 0 VALUE = {LIMIT (-0.001*V(214,216),0,-0.0002)} g4 0 14 VALUE = {LIMIT (0.002*V(217,218),1e-4,0)} *I=(0+0*V(219,220))+(0+0.2*V(217,218)) g5 6 2 VALUE = {LIMIT (0.002*V(217,218),5e-05,0)} i0 0 201 dc 0.001 i1 204 0 dc 0.001 i5 206 0 dc 0.001 i6 0 207 dc 0.001 r0 206 218 1 r1 220 0 1 v0 209 0 dc 1.9 v1 211 0 dc 1.6 v2 217 210 dc 0.2 v3 212 207 dc 0.025 v4 213 0 dc 1.6 v5 214 207 dc 0.025 v6 215 0 dc 0.6 v7 216 0 dc 1.7 .ENDS * * CMRR and PSRR Offset Generator * .SUBCKT ADCMP601_DVOS 12 13 17 2 6 e0 302 0 13 0 1 e1 304 0 12 0 1 g0 17 0 VALUE = {LIMIT (1.71e-06 - 3.3e-07*V(303,0),3e-06,-1e-06)} *I = 1.71e-06 -3.3e-07*V(303,0) g1 17 0 VALUE = {LIMIT (6.667e-07*V(6,301),2e-06,0)} r0 302 303 1000 r1 303 304 1000 v0 301 2 dc 2.5 .ENDS * * ESD Diodes * .SUBCKT ADCMP601_ESD 601 602 606 d0 601 606 DESD d1 602 601 DESD .ENDS * * Hysteresis and Latch Function * .SUBCKT ADCMP601_HYST 17 2 5 6 c0 410 409 3.4e-11 c1 401 0 1e-12 d0 0 404 DSIM1 d1 401 5 DSIM3 e0 402 405 405 403 1 e1 412 0 VALUE = {LIMIT (20*V(17,0),0.3,-0.3)} f1 6 0 VALUE = {LIMIT (7*I(v1),0.0007,0)} f2 0 2 VALUE = {LIMIT (8*I(v2),0.0008,0)} g0 408 17 VALUE = {LIMIT (0.01*V(410,409),0.0003,-0.0003)} g1 411 0 VALUE = {LIMIT (0.01*V(414,0),3e-4,0)} h0 413 0 VALUE = {LIMIT (1000*I(v0),0.030,0)} i2 403 0 dc 0.00125 i3 5 0 dc 1.25e-06 i5 0 405 dc 1e-06 q0 410 0 411 0 NPN_IN1 q1 409 412 411 0 NPN_IN1 r0 403 404 1000 r1 402 401 7500 r3 408 410 100 r4 408 409 100 r5 414 0 50 t0 413 0 414 0 z0=50 td=7e-10 v0 406 405 0 v1 407 406 0 v2 0 407 0 v4 408 0 dc 1 .ENDS * * Input Stage * .SUBCKT ADCMP601_INPUT 12 13 14 15 16 17 2 6 e0 101 0 0 2 -1 e1 102 0 0 6 -1 g0 102 17 poly(3) 108 107 106 105 104 103 0 0.01 0.01 0.01 q0 103 13 14 0 PNP_IN1 q1 104 12 14 0 PNP_IN1 q2 105 13 15 0 NPN_IN1 q3 106 12 15 0 NPN_IN1 q4 107 13 16 0 NPN_IN2 q5 108 12 16 0 NPN_IN2 r0 101 103 200 r1 101 104 200 r2 102 105 90 r3 102 106 90 r4 102 107 80 r5 102 108 80 .ENDS * * Output Stage * .SUBCKT ADCMP601_OUTPUT 1 2 21 6 c0 1 507 8.8e-13 c2 505 504 6e-14 c3 503 504 6e-14 d0 504 503 DSIM2 d1 505 504 DSIM2 d2 506 505 DSIM1 d3 503 501 DSIM1 e0 506 2 508 0 1 e1 6 501 502 0 1 e2 507 0 6 2 0.5 g0 0 505 VALUE = {LIMIT (-0.0042667*V(21,0),0.00032,-0.00032)} g1 503 0 VALUE = {LIMIT (0.0042667*V(21,0),0.00032,-0.00032)} g2 6 0 VALUE = {LIMIT (-0.0085333*V(21,0),0.00064,0)} g3 0 2 VALUE = {LIMIT (0.0085333*V(21,0),0.00064,0)} i4 0 508 dc 0.001 i5 0 502 dc 0.001 q0 504 505 2 2 NPN_OUT q1 504 503 6 2 PNP_OUT r0 1 507 50000 r1 504 1 10 r3 508 0 850 tc=-0.00302 r4 502 0 850 tc=-0.00302 .ENDS * * Models Used * .model DESD d cjo=5e-14 is=1e-17 rs=0.5 eg=1.12 .model DSIM1 d is=1e-12 .model DSIM2 d is=1e-14 eg=0.950 .model DSIM3 d is=1e-15 .model NPN_IN1 npn bf=140 cjc=1.20e-14 cje=2.78e-14 is=9.1e-18 rb=60 re=400 tf=4.7e-12 .model NPN_IN2 npn bf=1e6 cjc=1.20e-14 cje=2.78e-14 is=9.1e-18 rb=60 re=400 tf=4.7e-12 .model PNP_IN1 pnp bf=25 cjc=5.50e-14 cje=1.05e-13 is=3.5e-17 rb=75 re=600 tf=1.2e-12 .model NPN_OUT npn bf=75 cjc=1.60e-13 cjs=6.5e-14 is=1.0e-16 vaf=50 .model PNP_OUT pnp bf=60 cjc=1.50e-13 cjs=6.5e-14 is=6.4e-17 vaf=30
what is your email address?
cshappee@markem-imaje.com