Question about PCB design for efficient heat control of ADATE318

Hellow,

My customer is considering to use ADATE318 and for this, they should do the radiant heat design.

The say that they will use a heat sink at top sied of device and connected to EP (Exposed paddle).

And additionally, they are considering the design under bottom side of device.

They are considering to add a pad under bottom side of device and connect this pad to GND or VEE.

1) For more efficient heat control, what is your recommended design for preventing heat in below example?

      1. Use heat sink and add a pad which is connected to GND pins (GND pad).

      2. Use heat sink and add a pad which is connected to VEE pins (VEE pad).

      3. Use heat sink and don't add a pad under bottom side of device.

2) If you have better idea about preventing heat, would you advise how to design with ADATE318 to my customer?

3) And if you have a PCB design(layout) guide for ADATE318, would you share this guide to my customer?

Please advise me.

Regards,

Se-woong

Parents
  • Hi Se-woong,

       My Apologies on the very late reply,  I have run through our archives and I couldn't find any PCB design or layout guide regarding the ADATE318, I would still point to the Power Supply, Grounding, and Decoupling Strategy Section of the ADATE318 Datasheet Rev. B, Page 70 if they need a guide in that regard. With the better means of preventing heat, This would really be dependent on your application. The standard ofcourse is to use a relative large heatsink in a controlled, air cooled environment. Powering down unused blocks could be another way of doing this but again this is solely dependent of the end application.

Reply
  • Hi Se-woong,

       My Apologies on the very late reply,  I have run through our archives and I couldn't find any PCB design or layout guide regarding the ADATE318, I would still point to the Power Supply, Grounding, and Decoupling Strategy Section of the ADATE318 Datasheet Rev. B, Page 70 if they need a guide in that regard. With the better means of preventing heat, This would really be dependent on your application. The standard ofcourse is to use a relative large heatsink in a controlled, air cooled environment. Powering down unused blocks could be another way of doing this but again this is solely dependent of the end application.

Children
No Data