Frequency of input signal ADN2830

Dear engineer

At present, we are looking for a laser driver that can modulate the laser diode in the way of 100MHz sine wave + DC bias. At the same time, the chip needs to have APC function. From the data manual of adn2830, we know that adn2830 can modulate the continuous wave and has APC function, but the data manual does not indicate the frequency range of the received input signal. Can adn2830 work under such a high frequency signal? In addition, can this chip directly drive p-type laser diode. If not, whether there are other chip recommendations.