Post Go back to editing

MAT14 Cebo spefification

Hi All,

I received question mail from my customer as next.

The data sheet of MAT14 says that Cebo: 40pF typ at Vcb=15V, Ie=0, and f=1MHz.

My understanding of the Cebo is base-emitter capacitance at collector is open.

If my understanding is correct, why you state that Vcb=15V?

Mat04 says that Cebo: 40pF typ at Vbe=0V, Ic=0, f=1MHz, this seems reasonable condition.

Could you explain why Vcb=15V condition for the Cebo is stated?


Another question is the bulk resistance specification.

MAT14 rbe=0.4 ohm typ at 10uA<=Ic<=10mA.

For the MAT04, rbe=0.4ohm typ at 10uA<=Ic<=1mA

What is the main reason for this difference?


Best Regards,

Ricky