Post Go back to editing

ADN2892: SQUELCH pull-down value?

Hi,

I'm working with the ADN2892 for interfacing to a PIN diode with an integrated TIA.  The datasheet notes that you can use the LOS output to drive the SQUELCH input, which would disable the amplifier output when there is no optical signal input.  I have the ADN2892 evaluation board, and I've added a pullup from LOS to +3.3V.  I've verified that LOS is operating correctly, pulling to the correct level based on the optical input.

However, the SQUELCH pin is said to have a 100kohm pull down to GND according to the datasheet.  I've tried pulling this up to +3.3V with as little as 30 ohms, but it's stuck at GND.  Using the switch on the evaluation board, the SQUELCH pin has the correct behavior, but that's being pulled directly to +3.3V.  Am I missing something here or is the datasheet's description of this pin incorrect?

Thanks so much!

-John

  • Dear John,

    We are not 100% sure what you did and what you have observed.

    Would you please elaborate "I've tried pulling this up to +3.3V with as little as 30 ohms, but it's stuck at GND."

    Your experiment schematic might be useful for us to fully understand your observation.

    Did you control the ADN2892 SQUELCH input by using ADN2892 LOS output directly?

    If yes, did you connect ADN2892 LOS to SQUELCH pins directly with a fly line, after taken off switch S3?

    Please refer to Fig. 4 of AN-761 for the evaluation board circuit schematic details.

    One ADN2892 evaluation board will be useful to do these experiment. Glad you have one.

    Would you please share us your PD+TIA+ADN2892 schematic design for a review?

    To protect your proprietary design information, you may send your further questions

    and your PD+TIA+ADN2892 design schematic to me: dongfeng.zhao@analog.com.

    Best Regards,

    Dongfeng