Hello,
I recently purchased LTC1564. I wired it up according to the reference schematic given in the datasheet (Shown below)
Here are the things I tried
1. Single supply configuration
V+ = 5V
V- = GND
G3 = G2 = G1 = G0 = 0 (1V/V passband gain)
F3 = F1 = F0 = 0 , F2 = 1 (40kHz cutoff)
Input voltage: 1V p-p sine wave with frequencies ranging from 100Hz to 100kHz
2. Dual supply configuration
V+ = 5V
V- = -5V
G3 = G2 = G1 = G0 = 0 (1V/V passband gain)
F3 = F1 = F0 = 0 , F2 = 1 (40kHz cutoff)
Input voltage = 1V p-p sine wave with frequencies ranging from 100Hz to 100kHz
In both the configurations all I am getting on the output side is a 50mV p-p noisy signal having the same frequency as the input for the entire frequency range mentioned above.
What could be the reason for this issue? How should I go about fixing it?
tagged
[edited by: JValeriani at 1:59 PM (GMT 0) on 14 Oct 2019]