Article Where can I find a low power mode example for the MAX32650/51/52?

The MAX32650/51/52 SDK includes a low power mode example in the Applications sub-folder titled, LP.  The SDK/API can be downloaded using the ARMCortexToolchain installer.  You can easily choose to download only the product specific resources/firmware.  The folder is located in <MYINSTALLDIR>\Firmware\MAX32650\Applications\EvKitExamples\LP

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.