Article How far can the DS2482-100 1-Wire bus transmit?

The 1-Wire bus distance is not specified, but rather guidelines for capacitive loading are given and these should be followed to ensure a given bus length meets the requirements.

According to Note 2 on p.4 of the DS2482-100 datasheet:

With standard speed, the total capacitive load of the 1-Wire bus should not exceed 1nF. Otherwise, the passive pullup on threshold VIL1 may not be reached in the available time.

With overdrive speed, the capacitive load on the 1-Wire bus must not exceed 300pF

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.