Article Can two channel operation with two different references using the AD7124-8?

Yes, the AD7124-8 allows continuous conversions of two channels using different reference inputs. Configure one channel to use REFIN1+/- and another channel to use REFIN2+/-. The AD7124-8 supports multiple reference inputs, and in continuous conversion mode, it can automatically sequence through the enabled channels, performing conversions on each one.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.