Article Is it possible to get your EVAL-CN0566-RPIZ (Phaser) software to work with Kuiper Linux 2023\_r2?

Resolution:

Our software was written and tested with Kuiper Linux 2021_r2 which is available from https://swdownloads.analog.com/cse/kuiper/image_2023-04-02-ADI-Kuiper-full.zip .  It is not directly compatible with the latest Kuiper Linux 2023_r2 release because of a newer version of Matplotlib.  However, there are two options you can do to make our software work on 2023_r2:

  1. You can downgrade the version of numpy by running "sudo pip install --force-reinstall numpy==1.22".
  2. You can recompile pyadi-iio by navigating to the pyadi-iio directory and running "make dev".

Option 1 was recommended by our Phaser experts at https://ez.analog.com/adieducation/university-program/f/q-a/591123/software-for-eval-cn0566-rpiz-is-not-operational, while option 2 was said to work by an ADI customer in the same EngineerZone discussion.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.