TMC-5160 - Which power supply provides current for the gate driver?
The gate driver is supplied by the internal 12V regulator via pin 12VOUT. The gate current is only driven for a few 10 to a few 100ns in order to charge / discharge the MOSFET gates. So, with small MOSFETs, the mean current requirement is low (a few mA). But, with big MOSFETs at high supply voltage, it becomes significant for the internal regulator, and an external regulator is preferred.