Article What is the communication format of the Campbell (MAXREFDES4#) SPI? What is the command?

MAXREFDES4# uses the MAX11100 to transform the input voltage/current into digital signals. The SPI bus can be used to control the MAX11100. Please refer to the MAX11100 data sheet for the SPI communication data format and command.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.