Article Upon startup, there was a -200mV undershoot at the output voltage of MAX8902. What is the reason for this?

Under normal conditions, there should be no undershoot when MAX8902 turns on. The startup waveform can be seen on page 4 of the datasheet (rev 6 1/15) and is also shown below. The 200mV undershoot is possibly due to the load at the output. However, as long as the undershoot does not go beyond -300mV (absolute maximum rating as mentioned in the data sheet), it will not affect the chip operation, and will not damage the chip.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.