Article Does the MAX32660 have a unique identifier?

There is a unique serial number in the flash info block of the MAX32660.  It is stored in the first 24 bytes (0x40000-0x40017).  To read the information block you first must unlock it.  It is a good idea to lock it back when you're finished.  You can use the following two functions in flc.h to lock and unlock this block:

FLC_UnlockInfoBlock();

FLC_LockInfoBlock();

 
 
 
 

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.