Article Is there a Keil Device Family Pack (DFP) for the MAX32660?

Yes, there is a DFP available for the MAX32660.  It can be found at the following link*:

http://www.keil.com/dd2/maxim/max32660/

To use the MAX32660-EVSYS with the Keil IDE, you will need to change the debugger.  In Keil, go to Flash > Configure Flash Tools > Debug.  In the top right corner, change the debugger to CMSIS-DAP Debugger. 

 

* Link valid as of April 2019

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.