Article Do you have a USB mass storage device example for the MAX32650/51/52?

Yes, an example is provided in the SDK in the Applications sub-folder titled, USB_MassStorage.  The SDK/API can be downloaded using the ARMCortexToolchain installer.  You can easily choose to download only the product specific resources/firmware.  The folder is located in <MYINSTALLDIR>\Firmware\MAX32650\Applications\EvKitExamples\USB_MassStorage

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.