No, external capacitors are not needed on the 32KIN and 32KOUT pins. The 32KIN and 32KOUT pins have an internal capacitance of 6pF each. Therefore, only a 32.768kHz crystal (XTAL) should be connected to…
Yes, an example writting the flash is provided in the SDK in the Applications sub-folder titled, Flash. The SDK/API can be downloaded using the ARMCortexToolchain installer. You can easily choose to download…
Yes, an example is provided in the SDK in the Applications sub-folder titled, USB_CDCACM. The SDK/API can be downloaded using the ARMCortexToolchain installer. You can easily choose to download only the…
Yes, an example is provided in the SDK in the Applications sub-folder titled, USB_MassStorage. The SDK/API can be downloaded using the ARMCortexToolchain installer. You can easily choose to download only…
Yes, an RTC example is provided in the SDK in the Applications sub-folder titled, RTC. The SDK/API can be downloaded using the ARMCortexToolchain installer. You can easily choose to download only the product…
None of the MAX326XX family micros support the trace functionality and the ITM, TPIU, ETM, and HTM are not present. Keep in mind all the micros support access to the full debugger with breakpoint, single…
None of the MAX326XX family micros support the trace functionality and the ITM, TPIU, ETM, and HTM are not present. Keep in mind all the micros support access to the full debugger with breakpoint, single…