Article Can I use the MAX32631 EV Kit to evaluate a MAX32630?

Yes, the MAX32631 EV Kit contains a socket.  The MAX32631 which ships with the EV Kit can be removed.  This allows multiple devices to be programmed/evaluated, including MAX32630 and even the MAX32632.  The EV Kit only comes with one MAX32631, so additional samples must be procured separately.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.