This is correct, the MAX32620FTHR and MAX32630FTHR boards come with a programmer board and the 10 pin ribbon cable that is necessary to program the MCU. Most of the MAX32620FTHR boards come with the MAX32625PICO…
On the MAX32620FTHR, only the I2CM2 (P5_7/P6_0) has built-in pull-ups. The other ports do not! You have to use 4.7kOhm to 1.8V or 3.3V to utilize the other I²C buses.
The FTHR board has both the MAX32620 and MAX77650 chips (microprocessor and PMIC respectively).
The MAX77650 has a pin called PWR_HLD, and this pin has to be held high to keep the PMIC ON which in turn…
The FTHR board has both the MAX32620 and MAX77650 chips (microprocessor and PMIC respectively).
The MAX77650 has a pin called PWR_HLD, and this pin has to be held high to keep the PMIC ON which in turn…
To use a MAX32625PICO (as a programmer) to program a MAX32620FTHR, you will need to connect the MAX32625PICO and the MAX32620FTHR using a 10-pin ribbon cable that comes along in the kit. Then from the…
Microcontroller input pins, especially analog inputs, are very susceptible to EMI and that can cause erroneous results. One way to mitigate this is to use shielded cable, as the conductive shielding provides…
The charger built into the PMIC cannot automatically provide information to the LEDs. To do so your main application running on the MAX32620 has to handle the PMIC interrupt on the IRQ pin (C2), and after…
The FTHR boards use Li-ion Polymer batteries.
Here is the URL link for a compatible battery:
https://www.mouser.com/ProductDetail/Adafruit/1317?qs=%2Fha2pyFaduhNmwFKKfs2JwZ%252BqWiMUIC%2FMdqqgYKURGcBvUuwI8nakPGfPQNDf8ckNkfJEzBDAf54JaOKn…
The FTHR boards use Li-ion Polymer batteries.
Here is the URL link for a compatible battery:
https://www.mouser.com/ProductDetail/Adafruit/1317?qs=%2Fha2pyFaduhNmwFKKfs2JwZ%252BqWiMUIC%2FMdqqgYKURGcBvUuwI8nakPGfPQNDf8ckNkfJEzBDAf54JaOKn…