There are no known issues with lock up for the DS2482-100 device. That said, be careful with the 1-Wire master (any 1-Wire master) when connecting it to temperature sensors, EEPROM memories, or anything…
Yes, the I2C communication and the 1-wire IO communication are two separate protocols controlled by the Master (DS2482-100 in this case). The slave devices will only log data to the master when a request…
Yes, the I2C communication and the 1-wire IO communication are two separate protocols controlled by the Master (DS2482-100 in this case). The slave devices will only log data to the master when a request…
The datasheet is the governing document, so it should be correct also for 100kHz.
I2C timings are valid from 0 to 400kHz, per the fSCL EC table parameter. Keep in mind notes 11-15 also apply.
There is no need of an external pull-up resistor, please see description here:
The DS2482-100 is a self-timed 1-Wire master that supports advanced 1-Wire waveform features including standard and overdrive…
The 1-Wire bus distance is not specified, but rather guidelines for capacitive loading are given and these should be followed to ensure a given bus length meets the requirements.
According to Note 2…
The 1-Wire bus distance is not specified, but rather guidelines for capacitive loading are given and these should be followed to ensure a given bus length meets the requirements.
According to Note 2…
Most issues when not being able to get meaningful data from the DS2482-100 stem from corruption of the I2C protocol. For example, some microcontrollers will be programmed to send a stop command between…