ADUC814: FAQ

  • Created
  • Updated
Was this helpful?
  • ADUC814 minimum time and level for reset

    Question For ADUC814, what is the minimum time and level of the reset impulse I need to ensure a CPU reset? VDD is 4V. Answer The ADuC814 is specified for DVdd supply of 3V/5V (3V +/-10% and 5V +/…
  • ADuC814: Digital I/O configuration

    Question Can I program Port 1 and 3 as input or output, ie is it to send logic 1 or logic 0 via port 1 and 3? In the document, it says, whenever you write 0, it becomes input. It also says P1.2-P1…
  • ADUC814: Internal Temperature sensor specifications

    Question In the ADuC814 datasheet, it is mentioned that the internal temperature sensor of ADuC8xx gives 650mV at 25C and that "is a voltage output ... which is proportional to absolute temperature…
  • ADuC814: Temperature sensor

    Question The output of the temperature sensor is different (quite a lot) than that is mentioned in the datasheet for room temperature. May the sensor be broken down or do I have to make calibration…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.