Question Does ADSP-CM40x feature a Data Cache? Answer The 16KB cache inside ADSP-CM40x is designed to accelerate execution from flash
memory, which means that it is meant to act as a Code Cache. Because…
Question Are MEMX and MEMY physical memories? Answer No, these are only virtual memory that don't have any physical memory when
inside them. They are only translation memory regions which are used for…
Question Can I Perform flash programming in SPI Memory Mapped mode? Answer No, SPI Memory Mapped Mode only works with Read access. There is no write port
associated with it.
Question Can I Perform flash programming in SPI Memory Mapped mode? Answer No, SPI Memory Mapped Mode only works with Read access. There is no write port
associated with it.
Question Can I place DATA in CODE memory and vice-versa? Answer The ADSP-CM408F (an example package used for explanation) has 384KB of internal
SRAM memory that may be used as CODE or DATA. This is allowed…
Question Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain? Answer While there is no direct interface between the IAR Tool-chain and MATLAB or
Simulink, Mathworks offer the “Embedded…
Question How can I utilize Cache with Async memory connected SRAM? Answer SMC interfaced memory and Cache – how design works
A memory connected to SMC can be accessed directly from the system memory …
Question SPI/Cache :: Line-Wrap mode vs. Line-base-first mode. Which one to choose? Answer Wrap mode
Wrap mode is a specific feature supported by most flash devices in market. It
enables the host processor…
Question What do I need in order to evaluate the ADSP-CM40x Processors? Answer You need the following:
• The ADSP-CM408F EZLITE (for evaluation of the ADSP-CM407F and ADSP-CM408F
processors) or the…