Question How can I use the Blackfin processor intrinsic (built-in) functions? do you
have any documentation / example code on this? Answer Please use the VisualDSP On-line Help to obtain all the necessary…
Question We are looking for information on bus loading with the Blackfin BF533 device.
The goal is to use the emif with 4 external device (Flash / 2xsdram / duart (18
pf on this device));
On the…
Question We are looking for information on bus loading with the Blackfin BF533 device.
The goal is to use the emif with 4 external device (Flash / 2xsdram / duart (18
pf on this device));
On the…
Question I would like to connect my Blackfin EZ-Kit to a high speed converter (a few
MHz) over the PPI interface. Are there any extender cards available that can
help me with this? Answer The Blackfin…
Question We would like to connect the S1D13A05 EPSON device
(http://www.erd.epson.com/vdc/html/contents/S1D13A05.htm) to the ADSP-BF537
Blackfin Processor. How can I connect it? What is the best solution…
Question We would like to connect the S1D13A05 EPSON device
(http://www.erd.epson.com/vdc/html/contents/S1D13A05.htm) to the ADSP-BF537
Blackfin Processor. How can I connect it? What is the best solution…
Question How can we count Blackfin core clock cycles? CYCLES and CYCLES2 don't seem to
count anything (their value is always zero!) Answer The reason the cycle counter does not see to be working is because…
Question What are the differences between the ADSP-BF537 and the ADSP-BF533 booting
process? Answer There are some differences as explained in EE-261 "ADSP-BF537 Blackfin
Highlights for ADSP-BF533…
Question We would like to know how many cycles it will take the Blackfin processor to
perform a floating point operation (MAC, since, etc) by emulating 32-bit
floating point by way of an optimized…
Question Regarding the Blackfin processors, could you indicate the degradation in
performance resulting from a DSP programme, whose size exceeds the available
internal code memory space, not being…