ADN469xE: FAQ

  • Created
Was this helpful?
  • ADN469xE Evaluation Board

    Q Are there eval boards available, if so, is there anything unique about the ADN469xE eval boards? A There are two high performance evaluation boards available, the only ones available…
  • ADN469xE IBIS Models

    Q Are ADN469xE simulation models available? A Yes, IBIS models are available on the product pages. www.analog.com/MLVDS
  • ADN469xE: MLVDS and how is it different from B-LVDS and RS-485?

    Q What is MLVDS and how is it different from B-LVDS and RS-485? A MLVDS Stands for Multi-point LVDS (Low-Voltage-Differential-Signaling). It is standardized by the Telecommunications Industry…
  • ADN469xE: Rise and Fall Time matching Data Rate

    Q Why would I use a 100Mbps device instead of the 200Mbps device? A In transmission line theory, it is best practice to use a part with a rise and fall time as close to the data rate required…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.