ADN

  • Created
Was this helpful?
  • Ac coupling Vs Dc coupling

    Q When should I use ac-coupling vs. dc-coupling on the high-speed serial lanes? A Ac-coupling isolated the dc current between a transmitting Tx device and a receiving Rx device. This is useful…
  • ADN2685: could you send the final datasheet?

    Q Could you send us the final datasheet A This part never was released (status 11. Feb. 2014) only a preliminary datasheet was distributed. All efforts so far have been stopped to release the…
  • ADN2817 error correction

    Q My receiver signal may have some "errors" introduced due to various factors Can the ADN2817 be able to remove and "clean up the signal". Hence Can the CDR remove errors seen on its inputs…
  • ADN2820: Optical fiber communication

    Q Since our Institute deals with optical fiber communication we are interested in the following device: TIA ADN2820. Unfortunately I could not find an information on the 3dB bandwidth depending…
  • ADN2873: Minimum differential signal between the DATAP and DATAN

    Q The datasheet specification states a minimum differential signal between the DATAP and DATAN inputs of 0.4V. In practice the parts work well with a lower input differential swing. We would…
  • ADN2880: MAX leakage current specification of ADN2880 input

    Q Do you have the MAX leakage current specification of ADN2880 input(PIN2)? A ADN2880 is one of our high speed TIA device. Pin 2 is the photo-diode current input pin. In fact, all of the…
  • ADN2890/1/2 at 100Mbps?

    Question Can we use ADN2890, 2891, 2892 at 100Mbps? Is there an under limit? Answer The ADN2892 device supports operation from 1Gbps to 4.25 Gbps. The ADN2890 and ADN2891 are optimised for SONET applications…
  • ADN8834: Evaluation board difference

    Q We are interested in the ADN8834. What is the difference between ADN8834CB-EVALZ and ADN8834MB-EVALZ? Do you have any additional information or datasheet for the eval kits? A The…
  • AN-695 Q&A

    Q We have recently purchased an ADN8831 chip with the ADN8831 Eval-z evaluation board. We are currently trying to set up a TEC with a 10k NTC Thermistor module following the instructions given…
  • Can ADN4604 do single ended 75Ohm input and output?

    Q The ADN4604 device looks like it can be configured in single ended mode. Can it do single ended 75Ohm input and output? A The ADN4604 has internal 50-ohm termination single-ended resistors…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.