ADE7953: FAQ

  • Created
  • Updated
Was this helpful?
  • ADE7953 energy meter

    Question I have a doubt about the voltage to be applied to the input pins VP,VN ÷ IAP,IAN . The ADE7953 can be powered at 3.3Vdc and can accept ±250mV at IAP, IAN and ±500mV at VP, VN pins in single…
  • ADE7953 Sample code

    Question ADE7953 Sample code Answer Attached is a project written in C for a reference meter based on the ADE7953
  • Any tips or hints for the ADE7953 layout?

    Question We are using the ADE7953 and using very similar to your reference design, with a shunt and the only difference is that we have 4-layer layout and the power supply comes from the secondary…
  • How can we have LED to light-up when CF1 disabled (i.e. with no load)?

    Question Under our configuration, CF1 output are ‘1’ when CFx pulse mode is disabled. Could it be changed? When pulses are working, for our calibration frequency (1000 imp/kwh), CF is ‘1’ and pulse…
  • Simple single-phase voltage and current meter

    Question I am looking for a simple one phase voltage and current meter. Could you provide me with some simple solutions of your product? I would prefer minimal external network and small ic. Answer…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.