Question We are currently using an AD9959 DDS evaluation board. I am
interested in clocking the system using the external quartz option.
Could you please suggest an option for the quartz crystal? Answer…
Question Currently, we found the bandwidth of single tone output from frequency response
in the ADIsimDDS tool is 800KHz. Pls see the attached. Is it all right for such
wide bandwidth? Or is there…
Question I did an experiment of AD9959EVB. System Clock is 500MHz, FTW0 = 10MHz, FTW1 =
10.1MHz, use P0 Pin to switch the DAC's output frequency.When the switching
time is 20us, then the DDS's output…
Question Is the ballon a t Pin 8 & 9 required when using an oscillator to drive the
inputs or is the ballon just used to accommodate the mismatch of the external
clock input impedance on the Eval-board…
Question Hello, I am working on an application which needs two RF outputs at 80MHz witha programmable phase difference between them. The application is very sensitiveto phase noise between the two 80MHz…
The FTW resets the accumulator to its default state according to the registers listed in Table 32 of the datasheet. Enabling or disabling these registers can assist with the accumulator reset depending…
Question Data Valid Time (tDV) is indicated as 12ns minimum (refer to Table 25 On page
31 of the AD9959 RevB data-sheet. This can't be true with respect to the fast
5ns serial-data clock? Should it…
Question The AD9959's SYNC_CLK has no signal. What should I check to fix this? Answer The SYNC_CLK should be running by default in crystal REF CLK mode or in any
other REF CLK mode. However, the following…
Question The AD9959's SYNC_CLK has no signal. What should I check to fix this? Answer The SYNC_CLK should be running by default in crystal REF CLK mode or in any
other REF CLK mode. However, the following…