Question
In order to generate linear frequency modulation pulse signal, the AD9958 is able to output pulse signal when ACR[12]=0, but it is not whenACR[12]=1, and the SPI is in 4-Bit Serial Mode, what is the problem?
Answer
The amplitude can not be controlled when the SPI is in 2-Bit Serial Mode or 4-Bit Serial ModeFeedback: NO