AD9958: FAQ

  • Created
  • Updated
Was this helpful?
  • AD9958: Timing of SCLK for a data read operation

    Question Datasheet says that data is read at the falling edge of SCLK, but the timing diagrams are very unclear. The falling edges do not point to the read data bits properly. In table 25, the minimum…
  • AD9958_AmplitudeControl_in_Chirp_Mode

    Question In order to generate linear frequency modulation pulse signal, the AD9958 is able to output pulse signal when ACR[12]=0, but it is not whenACR[12]=1, and the SPI is in 4-Bit Serial Mode, what…
  • AD9958_profile pin error in datasheet

    Question In datasheet version 0 page 22: linear sweep mode,Profile pin 2 is dedicated to channel 0 and the Profile pin 3 is dedicated to channel 1, and so on.But in datasheet version A page 25: linear…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.