Question I would like to know what is the AD9954's power cunsumption for each state on
powerdown (refer to Table 9 of the datasheet, Rev.B Answer Please see estimated results attached for the AD9954…
Question The datasheet of the AD9954 specifies that DACBP should be decoupled to Ground.
It would make sense to me to decouple
it to the Analog Ground rather than the Digital Ground. It is not specified…
Question What is the RELATIVE level of the DDS ""spurious"" at DDS-Clock ( AD9954 at
400 MHz.) / 8 ,and DDS- Clock / 16 ?
( Ofcourse with no filtering but direct at R-DAC and single ended oputput )…
Question In the RAM continuous recirculate mode, what is the phase information at the
very beginning of each sweep cycle? Does the phase reset to 0 at the beginning
of each sweep cycle? Answer The…
Question In the RAM continuous recirculate mode, what is the phase information at the
very beginning of each sweep cycle? Does the phase reset to 0 at the beginning
of each sweep cycle? Answer The…
Question I have used AD9954 as a clock reference, but in the output of DDS, one spur
which frequency is N*Fxtal/4 (N is the PLL multiplier)exists, would you help me
how to eliminate this spur. Answer…
Question I have used AD9954 as a clock reference, but in the output of DDS, one spur
which frequency is N*Fxtal/4 (N is the PLL multiplier)exists, would you help me
how to eliminate this spur. Answer…
Question 1.Our design uses the two options described on datasheet page 30. I.e.
synchronizing with SYNC_IN and SYNC_CLK signals AND a single crystal driving
multiple (=16) AD9954s. Do you recommend…
Question What is the relationship between the power consumption and the frequency of the
system clock? Answer Please refer to the results in the attached file.
Question I have an evaluation board AD9954/PCBZ,but i didn't find a connection cable to the PC. So what type of cable should I usewhere I can find it? Answer The cable is not provided by Analog Devices…